Test Wi-Fi with companion IC CC3351 for RF testing with PC tools
See required hardware, software, and tools to evaluate RF performance of the CC33xx devices with PC tools.
评估板
BP-CC3351 — SimpleLink™ CC3351 dual-band Wi-Fi 6 and Bluetooth® Low Energy BoosterPack™ plug-in module
BP-CC3351 — SimpleLink™ CC3351 dual-band Wi-Fi 6 and Bluetooth® Low Energy BoosterPack™ plug-in module
版本: null
发布日期:
LP-XDS110ET — XDS110ET 具有 EnergyTrace™ 软件的 LaunchPad™ 开发套件调试器
版本: null
发布日期:
应用软件和框架
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi 工具箱是一个用于帮助开发和测试 CC33xx 和 CC35xxE 器件的工具集。
None.
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi 工具箱是一个用于帮助开发和测试 CC33xx 和 CC35xxE 器件的工具集。
版本: 4.1.8
发布日期: 2026-2-11
Windows Installer
SHA-256 校验和
Linux Installer
SHA-256 校验和
macOS Intel Ventura Installer
SHA-256 校验和
macOS Arm64 Ventura Installer
SHA-256 校验和
产品
Wi-Fi 产品
硬件开发
评估板
文档
Manifest
发布信息
SimpleLink Wi-Fi Toolbox is a comprehensive cross-platform development suite that delivers essential tools for streamlined development and rapid prototyping with the CC33XX and CC35XXE wireless connectivity solutions.
This is version 4.1.8 of the SimpleLink Wi-Fi Toolbox.
Previous release was 4.0.13
新增功能
- [Programmer] New Flash supporting: [Experimental] Winbond W25Q12PW
- [Programmer] Production Line support -> Memory Validation Test (renamed from Calibration Test)
- [Programmer] TI Wireless Firmware configuration file required to build application image
- [Programmer] Support “no OTA” option for Flash larger than 4MB
- [Programmer] Default selection for Flash type changed to IS25WJ064F and “Enable OTA” enabled by default.
- [Radio Tool] Additional BLE TX power configurations ( -23dBm )
- [General] Updated Toolbox User Guide
- [CLI] New and updated commands (refer to full release notes for details)
- [All] Bugfixes and enhancements
应用软件和框架
SIMPLELINK-CONNECT — SimpleLink Connect App for the SimpleLink Low Power SDKs
using BLE feature.
支持的产品和硬件
产品
Sub-1GHz 无线 MCU
Wi-Fi 产品
低功耗 2.4GHz 产品
硬件开发
开发套件
评估板
SIMPLELINK-CONNECT — SimpleLink Connect App for the SimpleLink Low Power SDKs
版本: 1.3.6
发布日期: 2024-7-31
Apple App Store
Google App Store
产品
Sub-1GHz 无线 MCU
Wi-Fi 产品
低功耗 2.4GHz 产品
硬件开发
开发套件
评估板
发布信息
The SimpleLink Connect Mobile app is an example Bluetooth® Low Energy application for mobile devices that works with:
- CC13xx and CC26xx devices running the SimpleLink Low Power SDK
- CC33xx devices attached to a host running the CC33XX Software.
The app provides a baseline for users to quickly build their own mobile apps, using iOS or Android. Source code is provided enabling easy customization.
Features:
- iOS compatible Bluetooth® Low Energy phone app and source code
- Android™ compatibly Bluetooth® Low Energy phone app and source code
新增功能
- Dedicated screens for CGM profile, Glucose profile, and Wi-Fi Provisioning over BLE.
- Option to filter the scan list by service UUID and by BD address.
- Revised navigation flow to directly access the service-specific screen, with an option to switch back to the characteristic view.
- Ability to configure a generic URL as the firmware repository, not limited to GitHub.
- Updated settings view with configuration options separated into different screens.