Get started on CC330x with RTOS
BP-CC3301 — SimpleLink™ CC3301 Wi-Fi 6 and Bluetooth® Low Energy BoosterPack™ plug-in module
BP-CC3301 — SimpleLink™ CC3301 Wi-Fi 6 and Bluetooth® Low Energy BoosterPack™ plug-in module
LP-AM243 — AM243x general purpose LaunchPad™ development kit for Arm®-based MCU
LP-AM243 — AM243x general purpose LaunchPad™ development kit for Arm®-based MCU
CC33XX-RTOS-MCU — CC33xx device driver for MCU and RTOS platforms
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
CC33XX-RTOS-MCU — CC33xx device driver for MCU and RTOS platforms
CC33xx RTOS MCU installer for Linux
CC33xx RTOS MCU installer for Windows
产品
Wi-Fi 产品
硬件开发
评估板
文档
Manifest
发布信息
This CC33xx RTOS MCU Software Package delivers components that enable engineers to develop applications on the Texas Instruments CC33xx Wi-Fi devices and Sitara family of microcontrollers (MCU).
This software toolkit provides the drivers for CC33xx devices to be used with a Real-Time Operating System (RTOS) on a microcontroller.
This is version R7.1 of the CC33xx RTOS MCU Software Package.
新增功能
- Updated to latest RAM bootloader (was 1.0.0.26)
- Added support for station regulatory domain
- Configuring regulatory domain is done by using the Wlan_RoleUp() Command/API with EU,US,JP,CSI(custom) as a parameter.
- For custom fields, use Wlan_Set with the WLAN_SET_CUSTOM_DOMAIN_ENTRY
- More information is in the wlan_if.h file
- Scan mechanism improvements
- General bugs fixes
- Multi Role Fixes
- Interoperability improvements
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi Toolbox collection of tools to help development and testing of the CC33xx
支持的产品和硬件
产品
Wi-Fi 产品
硬件开发
评估板
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi Toolbox collection of tools to help development and testing of the CC33xx
SimpleLink Wi-Fi Toolbox Windows Installer
SimpleLink Wi-Fi Toolbox Linux Installer
SimpleLink Wi-Fi Toolbox MacOS Installer
SimpleLink Wi-Fi Toolbox Intel based MacOS Installer
产品
Wi-Fi 产品
硬件开发
评估板
文档
Manifest
发布信息
SimpleLink Wi-Fi Toolbox is a cross-platform software kit, that provides all required tools for fast and easy ramp-up of the CC33xx family of devices. One of the included tools is Radio Tool.
Radio Tool is a tool for RF evaluation and testing of CC33xx designs, during development and certification. The tool enables low-level radio testing capabilities by manually setting the radio into transmit or receive modes. Usage of the tool requires familiarity and knowledge of radio circuit theory and radio test methods.
This is version 2.5.5 of the SimpleLink Wi-Fi Toolbox.
Previous release was 2.4.7
新增功能
- CC3301MOD / CC3351MOD support added
- UI changes - New "Region" selection and part of Radio Tool intro
- Update TI Wireless Firmaware 1.7.0.32x
- Optimized download time via SWD, follow README in <Install_DIR>/radio-tool-binaries-<cc33xx>/FAS_MODE_README.md
- Bug fixes