SLUAAT9 January 2024 LM2005 , LM2101 , LM2103 , LM2104 , LM2105 , LM25101 , LM5100A , LM5100B , LM5100C , LM5101A , LM5101B , LM5101C , LM5102 , LM5104 , LM5105 , LM5106 , LM5107 , LM5108 , LM5109A , LM5109B , LM5109B-Q1 , LM5113-Q1 , SM72295 , SM74104 , UCC27200 , UCC27200-Q1 , UCC27200A , UCC27201 , UCC27201A , UCC27201A-Q1 , UCC27211 , UCC27211A , UCC27211A-Q1 , UCC27212 , UCC27212A-Q1 , UCC27282 , UCC27282-Q1 , UCC27284 , UCC27284-Q1 , UCC27288 , UCC27289 , UCC27301A , UCC27301A-Q1 , UCC27302A , UCC27302A-Q1 , UCC27311A , UCC27311A-Q1
Bidirectional buck-boost converters are used in applications such as electric vehicles DC-DC converters at high power and output current levels (>200A load). These multi-phase DC-DC converters are common in the 48V to 12V power systems found in mild hybrid automotive applications. These designs are typically multi-phase systems with the ability to enable and disable phases to optimize efficiency in different operating modes of the controller. These different operating modes pose unique operating conditions for the gate drivers that the designer needs to be aware of. The 100V half-bridge gate drivers are used in various high power, high power density applications with a 48V bus. These drivers are commonly used in the bidirectional DC-DC power systems and are the focus of this application note. This paper cover unique operational challenges with respect to driver bootstrap bias operation for gate drivers in the multi-phase buck-boost power systems used in automotive as well as grid power systems.
All trademarks are the property of their respective owners.
To maintain proper expected operation of the power converter, one must understand the start-up sequence of the half-bridge driver especially if using a bootstrap bias for the floating high-side driver. Some designers possibly may not be aware of the timing sequence of the half-bridge driver IC unless the designers encounter issues with the converter operation. For the driver outputs to respond to the LI (low-side) and HI (high-side) inputs, the VDD voltage level must be above the rising VDD UVLO (under voltage lockout) threshold. After the VDD UVLO threshold is satisfied there is a UVLO delay time before the outputs responds to the driver inputs. There is also a UVLO on the HB (high-side) bias, so the HB bias must be well above the rising HB UVLO threshold for the HO output to respond to the HI input. The HB UVLO circuit also has a delay time before the HO (high-side driver output) responds to the HI input.
To better understand the concerns of driver startup in a bidirectional DC-DC converter, we look at the driver start-up sequence in a standard DC-DC synchronous buck starting at 0V on the output as a reference.
The preferred startup sequence for the driver is to have VDD rise and well above the UVLO threshold before the PWM signals for LI and HI start. Since there is a UVLO delay on VDD, we recommend a delay of 10us or longer from VDD rising to the PWM signal start. In the typical synchronous buck with the output starting at 0V, there is a path from VDD through the boot diode to HB to charge the HB capacitor. This capacitor is charged when HS is close to ground which is the case at startup since VOUT is 0V and the output inductor provides a path from HS to ground, refer to Figure 1-1. The HB to HS capacitor charges at the same time that VDD is rising due to this path to the output which starts at 0V. Once VDD is above the UVLO threshold and HB-HS is above the UVLO threshold for 5-10us for most typical half-bridge drivers, the LO and HO outputs respond to the LI and HI inputs. Regarding the HB floating bias bootstrap circuit, the forward current in the driver boot diode typically has low forward current assuming the VDD rise time dV/dt is low which is the case in most systems. Typically, the bootstrap capacitor is fully charged before switching begins in the driver and power stage. Figure 1-2 shows this sequencing as well as how HS voltage rises to reverse bias the bootstrap diode.With bidirectional DC-DC converters many applications have multi-phase synchronous buck-boost to support high current outputs. A common practice to increase efficiency at lighter loads is to disable phases as the output current/power is decreased. Figure 1-3 illustrates a 2-phase configuration with one phase active and one in the inactive state. In practice there can be additional phases in the converter. In this case there is 12V on the output supplied by the active phase and the 2nd phase has the 12V output on the power stage switch node. On the inactive phase, the driver IC HS pin is at 12V which prevents the boot capacitor from charging assuming VDD is 12V or less. When the inactive phase starts switching the 1st LI input turns on the low side FET providing the charging path for the boot capacitor current (IHB) through the boot diode. Also, negative inductor current starts flowing from the 12V output through the low side FET as well. With 12V applied to the boot diode anode and high dV/dt on the HS pin, there is high initial boot diode forward current flowing. In many applications this can exceed 10A and significantly higher depending on the driver IC boot diode dynamic resistance. If the PWM pulses to the idle phase are enabled such that there is a short initial LO pulse, the forward current in the boot diode can be very high at the time the low side turns off. With 12V on the converter output there is negative current ramping in the output inductor when LO turns off. This negative inductor current results in the switch node transitioning high and clamping to the 48V input. This forces off the boot diode with high forward current flowing which results in potentially high reverse current in the boot diode. This reverse recovery stress can damage the internal boot diode.