• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Circuit Board Insulation Design According to IEC60664 for Motor Drive Application

    • SLUAAR5 august   2023 ISO5451 , ISO5452 , ISO5851 , ISO5852S , ISO7741 , ISO7810 , ISO7820 , ISO7821 , ISO7830 , ISO7831 , ISO7840 , ISO7841 , ISO7842 , UCC23513 , UCC5310 , UCC5320 , UCC5350 , UCC5390

       

  • CONTENTS
  • SEARCH
  • Circuit Board Insulation Design According to IEC60664 for Motor Drive Application
  1.   1
  2.   Abstract
  3. 1Introduction of Key Terms in IEC60664
    1. 1.1 Clearance and Creepage
    2. 1.2 Insulation Type
    3. 1.3 Decisive Voltage Class and Extra-Low Voltage
    4. 1.4 Protection Class
    5. 1.5 Pollution Degree
    6. 1.6 Overvoltage Category
    7. 1.7 System Voltage
    8. 1.8 Working Voltage and Voltage Block
  4. 2Insulation Distance Definition
    1. 2.1 Clearance and Creepage Determining Process
    2. 2.2 Clearance and Creepage Determining Method Example
  5. 3Summary
  6. 4Reference
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Technical White Paper

Circuit Board Insulation Design According to IEC60664 for Motor Drive Application

Abstract

The International Electrotechnical Commission (IEC) standard IEC 60664: Insulation coordination for equipment within low-voltage systems specifies the requirement for clearances, creepage distances, and solid insulation for equipment based upon their performance criteria.

Motor drive systems typically consist of high-voltage and low-voltage subsystems. Such systems demand reliable galvanic isolation to isolate high-voltage circuits from low-voltage circuits.

To better assimilate the method to calculate the insulation distances when designing the circuit board in motor drive system, this document aims to present the insulation design guide and example to meet the requirement coming from IEC60664-1.

1 Introduction of Key Terms in IEC60664

1.1 Clearance and Creepage

Clearance: Defined as the shortest distance between two conductive materials measured through air. Sufficient clearance distance prevents an ionization of the air gap and a subsequent flashover. Similar to creepage distance the pollution degree, temperature and relative humidity influence the tendency for a breakdown. Breakdown along a clearance path is a fast phenomenon where damage can be caused by a very short duration impulse. Therefore, it is the maximum peak voltage, including transients (overvoltage category [OVC] level), that is to be used to determine the required clearance spacing. Figure 1-1 shows the definition of clearance.

GUID-20230825-SS0I-CKDQ-QTTR-QGW7KQX0MG63-low.svg Figure 1-1 Definition of Clearance

Creepage: Defined as the shortest path between two conductive materials measured along the surface of an isolator which is in between. Maintaining a certain creepage distance addresses the risk of tracking failures over lifetime. The generation of a conductive path along the isolator surface due to the high voltage applied over time is related to the root mean square (RMS) value and depends on environmental conditions, which are described by a pollution degree and the material characteristics of the isolator comparative tracking index (CTI). Breakdown of the creepage distance is a slow phenomenon determined by DC or RMS voltage rather than peak events or transients. Inadequate creepage spacings can last for days, weeks or even months before failure. Figure 1-2 shows the definition of creepage.

GUID-20230825-SS0I-ZHJF-KZ1Q-MRFGCH5WRK3F-low.svg Figure 1-2 Definition of Creepage

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale