• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Bulk up Your 24-VDC Power Distribution with Industrial High-side Switches

    • SSZT168 may   2021 TPS272C45 , TPS274160 , TPS27S100 , TPS27SA08

       

  • CONTENTS
  • SEARCH
  • Bulk up Your 24-VDC Power Distribution with Industrial High-side Switches
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Bulk up Your 24-VDC Power Distribution with Industrial High-side Switches

Paul Kundmueller

For athletes to perform at their highest level – to run a mile in less than five minutes or leap into the air and dunk a basketball – they need strong muscles. The heart supplies blood through the veins to the muscles to enable movements such as gripping an object with your hand or moving a finger when your brain instructs it to. But without muscles, these spectacular feats would not possible.

Similarly, factory floors use a 24-VDC power network to distribute power from power supplies (the heart) through wires and connectors (the veins) to different power switches (the muscles), enabling the movement of relays, actuators and sensors when the programmable logic controller (the brain) tells them to do so. This is evident in large machine tools that use power switches to internally transfer 24 V of power – from board to board, or externally in digital output and remote input/output modules – to distribute power to relays, actuators and sensors. These power switches enable robots, motor drives and other large machine tools to automate a factory to perform tasks at a high speed and with precision – much like the athletes we love to watch. Figure 1 is a visual representation of a factory illustrating the use of power switches in different types of factory automation equipment.

GUID-003BC44E-4BEC-4AE1-82AC-7C0C5A60D675-low.png Figure 1 Illustration of Power Switches in Different Factory Automation Equipment

So what type of semiconductor devices act as the muscles in a factory environment? Industrial high-side switches from TI go beyond just distributing power and drive output loads – they also provide protection and diagnostic capabilities to prevent extended factory downtimes. For example, the switches include features such as:

  • Adjustable current limiting for short-circuit and overload conditions.
  • Integrated current sensing for load diagnostics, thus reducing downtime.
  • Open-load detection for wire breaks.
  • An integrated drain-to-source voltage (VDS) clamp for inductive load driving.

One of the most important protections is current limiting, which helps keep factory automation systems with board-to-board connections and offboard loads from experiencing significant downtime due to short-circuits, which could be caused by condensation/humidity, wire breaks or short-to-ground scenarios. TI’s high-side switches also have the option for an external resistor to adjust the current limit, offering added flexibility. This flexibility makes it possible to use the same switch across a variety of output load conditions. There is no need to buy an additional device; simply change an external resistor to get a new current-limit value. Figure 2 is a block diagram of a dual-channel high-side switch with independent adjustable current limits for each of its output channels.

GUID-8116D431-1287-44C5-81B7-953DDF94A972-low.png Figure 2 Dual-channel High-side Switch, TPS272C45

Integrated current sensing offers the ability to sense the amount of current flowing through the high-side switch, which can be invaluable when debugging a machine that’s not working properly.

The switches output a current onto an external resistor that is proportional to the current passing through the internal power metal-oxide semiconductor field-effect transistor, which can then be fed to an analog-to-digital converter (ADC) in the system for processing.

Current sensing enables users to diagnose open-load situations if a wire were to break or become unplugged in a machine. This can greatly reduce debugging time for large machines that have many outputs or board-to-board connections by enabling technicians to better pinpoint which system may have the broken or missing wire, and get the system up and running again.

Additionally, current sensing can help determine whether a system is experiencing an overcurrent event or drawing an unexpected amount of current. This can alert technicians to bring a spare load or subsystem to replace the faulty one.

Providing feedback to the system that a certain load has turned on correctly is another benefit of current sensing. There are loads, such as a solenoid actuator, which have a very distinct input current profile. A typical current profile for a solenoid actuator is shown in Figure 3 below and has three components to it; a stall current, a notch current and a holding current. This profile can be captured by the high-side switches current sensing and sent to an ADC for analysis. This analysis can help to provide a feedback mechanism to the system, indicating that the load it’s powering did indeed turn on correctly and the system is running as expected.

GUID-E8189F8B-6709-440F-A3C3-10E850294744-low.png Figure 3 Output Current Profile of a Solenoid Actuator Captured by Current Sense of TPS274160

TI industrial high-side switches not only provide more muscle power with low drain-to-source on-resistance RDS(ON) solutions; they also provide flexibility and intelligence in your factory systems to enable more reuse and less downtime. TI is continuing to build out its industrial high-side switch portfolio with lower RDS(ON) switches, more feature integration and higher channel counts.

Additional Resources

  • Review the following data sheets, which describe the capabilities of high-side switches for use in industrial applications:
    • “TPS272C45 45-mΩ, Dual-Channel Smart High-Side Switch with Diagnostics.”
    • “TPS27S100x 40-V, 4-A, 80-mΩ Single-Channel High-Side Switch.”
    • “TPS274160x 160-mΩ Quad-Channel Smart High-Side Switch.”
    • “TPS27SA08 36-V, 10-A, Single-Channel Smart High Side Switch.”
  • Review the following application reports, which describe the use of high-side switches in factory automation and motor drive systems:
    • “Enabling SPI Communication Using TI's Smart High Side Switches.”
    • “TPS272C45 Enables Smart Power Management of Remote I/Os.”

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale