SLVAFJ0 april 2023 TPS650350-Q1 , TPS650352-Q1
This application note provides a summary of the CISPR-25 Conducted and Radiated Emissions test results using the TPS650350-Q1 Power Management Integrated Circuit (PMIC) for automotive camera applications. This device is capable of passing CISPR-25 and other automotive electromagnetic-compatibility (EMC) test specifications. Similar results can be achieved using other devices in the TPS65035x-Q1 family. Due to an advanced spread spectrum clocking (SSC) feature, these devices can pass EMC tests without needing a fully-optimized layout, allowing for more flexible component placement and routing as required by the camera application.
All trademarks are the property of their respective owners.
This application report illustrates the EMI/EMC performance of the TPS650350-Q1 and relevant circuits in automotive applications using example schematics and layout design. With this example, the TPS650350-Q1 and associated components pass the CISPR-25 Vehicles, boats and internal combustion engines – Radio disturbance characteristics – Limits and methods of measurement for the protection of on-board receivers conducted emission in the 0.15 MHz to 108 MHz frequency range, and radiated emission in the 0.15 MHz to 1000 MHz frequency range.
The TPS650350-Q1, TPS650351-Q1, TPS650352-Q1, and TPS650353-Q1 are a family of PMICs for camera applications. Each device includes three step-down (buck) converters and one low dropout (LDO) regulator. The three buck converters are capable of spread spectrum clocking (SSC), a feature that modulates the switching frequency of each converter to spread the power that can cause EMI. This internal modulation spreads the operating frequency from 2.0 MHz to 2.5 MHz with a center frequency of 2.25 MHz and can be enabled or disabled with a single register write through I2C communication.
The goal of spread spectrum architecture is to spread out emitted RF energy over a larger frequency range. Spreading the operating frequency of the buck converters results in a more continuous power spectra that is lower in peak amplitude, as shown in Figure 2-1. This peak reduction is possible because the time integral of the curve (the EMI energy emitted by the circuit) remains constant whether spread spectrum is enabled or disabled.
Figure 2-2 compares the conducted emission performance with SSC enabled and disabled using the TPS650350-Q1 and the example layout discussed in this application report.