• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Power Amplifiers for Constant Voltage Audio Systems

    • SLAA898 September   2022 TAS3251 , TPA3255

       

  • CONTENTS
  • SEARCH
  • Power Amplifiers for Constant Voltage Audio Systems
  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Power Amplifiers
    2. 1.2 Discrete Power Amplifier Implementation
    3. 1.3 Class-D Amplifier Implementation
    4. 1.4 Advantage of a Class-D Implementation
  4. 2Background
    1. 2.1 Why Use Constant Voltage Audio Systems
    2. 2.2 Basic Principle of Constant Voltage Systems
    3. 2.3 Power Loss in Transformer
    4. 2.4 Auto-Transformer
  5. 3System Test (Based on TPA3255)
    1. 3.1 Transformer Characteristics
      1. 3.1.1 Turns Ratio and Resistance Match
      2. 3.1.2 DCR of the Transformer
    2. 3.2 System Build-Up
    3. 3.3 System Test
  6. 4Efficiency Analysis and Optimization
    1. 4.1 Efficiency of Three Parts
      1. 4.1.1 Efficiency for TPA3255
      2. 4.1.2 Efficiency for Step-Up Transformer
      3. 4.1.3 Efficiency for Step-Down Transformer 330-040
    2. 4.2 Improvements on System Efficiency
      1. 4.2.1 Improve Resistance Matching
      2. 4.2.2 Apply a Transformer With Less Power Loss
  7. 5Considerations on Building a Constant Voltage System
    1. 5.1 Transformer Saturation
    2. 5.2 Low DCR
    3. 5.3 Resistance Matching
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Power Amplifiers for Constant Voltage Audio Systems

Abstract

Constant voltage audio systems are commonly used in installations where audio information needs to be distributed over long and varied distances to many different points of load with high total power delivery. These systems are widely used in commercial building installations for public announcement (PA) or for fire safety and building security notifications by specific zone. This application note describes the operation of constant voltage audio systems and derives the equations needed to determine overall system efficiency. Advantages of integrated power amplifiers, such as the TPA3255, compared to traditional discrete amplifier implementations are discussed. An example system was built using the TPA3255 and measurements were taken with different audio transformers to show the impact that different transformer parameters have on overall system efficiency.

Trademarks

Peavey® is a registered trademark of Peavey Electronics Corp.

EDCOR® is a registered trademark of EDCOR Electronics Corporation .

All trademarks are the property of their respective owners.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale