• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Who Tampered with My PLC? Are Industrial Control Systems Too Flexible?

    • SSZTB13 august   2016 CSD18532Q5B , ISO7141CC , ISO7141FCC , ISO7421 , LM5009 , LM5050-1 , LM5069 , MSP430F2112 , TLC5928 , TPS1H100-Q1

       

  • CONTENTS
  • SEARCH
  • Who Tampered with My PLC? Are Industrial Control Systems Too Flexible?
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Who Tampered with My PLC? Are Industrial Control Systems Too Flexible?

Ingolf Frank

GUID-6E9E21E8-E895-4F8D-9C79-DE29E9BD9AC9-low.jpg

Many (if not most) machines are controlled by specialized computers called programmable logic controllers (PLCs). The roots of this trend reach back into the late 1960s when machines and assembly lines became increasingly complex, as did their corresponding control systems. The hard-wired relay-based control systems of that time were inflexible and error-prone. Maintenance was a nightmare. The horrendous amount of required relays and cabling didn’t make engineer’s lives easier. Mechanical devices like relays simply wear out much faster than well-designed electronic devices. To optimize the control systems of their assembly lines for better reliability and maintenance General Motors contracted Bedford Associates to design an electronic replacement for the various hard-wired relay based control systems. The first PLC was born. Called the MODICON-084, it is today considered the grandfather of all PLC systems. This revolutionary technology was quickly adopted industry-wide because of its flexibility, simplicity and better cost structure.

In the following years PLCs shrunk to smaller form factors and programming became easier. More PLC vendors appeared and a standardization of the programming and feature sets occurred. Today there is a large infrastructure of PLC systems with functions and features for nearly all situations in automation and process control.

The main benefits of PLC-based control systems namely flexibility and simplicity might now motivate the user of a machine to optimize his work flow. Changing the software can increase machine speeds or reduce the cycle time of a production process. Time is money! As a consequence, however, machines wear out more quickly. They could even enter dangerous states because two process steps may collide when the waiting time in-between is too short. Changing the hardware may also appear attractive. Let’s assume that we have a machine function that happens at a specific time – why not wire an extra fan to the digital output controlling this function if that process step needs some additional cooling? As long as we don’t violate the specified parameters of that output it is not really a problem, but what if we do violate the parameters and the machine gets damaged or ages faster? While it is possible for the machine manufacturer to block unauthorized access to key software functions, it is rather difficult to block access to the screw terminals of PLC I/O modules.

Once the hardware tinkering has been removed again it is impossible to prove. The machine’s manufacturer may be blamed for the damage to the output module or even the mechanical parts of the machine though it is not his fault at all. What can he do to get at least an indication of such tampering? Since we live in the age of electronics, there should be an electronic solution.

GUID-04BD8253-FE93-44F3-8FDD-6E05CB494517-low.jpg

The 8-Channel 1A/Ch High Side Driver for Programmable Logic Controller Reference Design (TIDA-00183) can record output currents and compare them in real time with a stored reference. Each of the 1A outputs has a function to measure the output current. Every type of load has a specific current pattern when switched on. A classic light bulb, for example, starts with a current 10 times as high as its average current during operation. A relay begins with a soft current, which then increases to its operational level. A motor starts with a high current peak but then settles to a level corresponding to its mechanical loading.

How can the manufacturer apply this current recording function to protect the machine and also conduct some forensics when damage happened? The controlling PLC knows when it turns on and off a load. The machine’s designer knows what type of load is connected to which output. These two pieces of information, together with current sensing, enable the PLC to verify the connected loads in real time. Alternatively the machine could record the current patterns of all connected loads during the end test of the machine before shipment and store the patterns for later reference and verification. This verification not only makes unauthorized modifications visible, but also the effects of aging and defective loads. In many cases, the machine can then inform the operator early enough that the machine will break or has been modified by unauthorized personnel.

The current-sensing feature demonstrated in TIDA-00183 can even do more. It enables the implementation of soft fuses, which are software-configurable protection schemes specifically tailored to the connected load. Also load balancing could be realized; if one output needs more current than the output quota of 1A but a couple of others need less, the PLC can adjust the current limits accordingly as long as the sum of currents stays under the module limit. These functions help achieve a level of functionality and diagnostics that simply haven’t existed before.

Additional Resources

  • Find more information about end-equipment solutions for PLCs.
  • Check out TI's factory automation overview for reference designs and product solutions.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale