Mioty technology is a new low-power wide-area network (LPWAN) solution, and is a true standardized technology based on ETSI 103 357. Mioty achieves long range with Sub-1 GHz communication, and offers robust networks due to its innovative telegram splitting. It is also capable of scaling to thousands of devices on a single base station. Target applications are ultra-low power sensor devices, such as metering and environmental/industrial monitoring. These sensor devices can have a battery lifetime beyond 10 years in a Mioty network.
Why choose TI for mioty?
Getting started
Mioty provides communication for large-scale deployments to ensure reliable and efficient transmission in challenging environments, making this protocol suitable for long-range, low-power and highly scalable applications.
To start building your own network, follow these steps:
MIOTY 技術的協定軟體
使用 LaunchPad SensorTag 套件,開始評估 MIOTY® 協定軟體:
- 購買一個或多個 CC1352R SensorTag 套件
- 購買一個 CC1352R1 LaunchPad 開發套件
- 下載 SimpleLink™ 軟體開發套件
- 如需開發 MIOTY 堆疊,請聯絡 Stackforce
- 向 MIOTY 訂購閘道
MIOTY 技術為新型低功率廣域網路 (LPWAN) 解決方案,且是以 ETSI 103 357 為基礎的真正標準化技術。MIOTY 透過 Sub-1 GHz 通訊實現長距離通訊範圍,且由於採用創新的電報拆分 (telegram splitting) (...)
SimpleLink™ 多頻帶 CC1352R 無線 MCU Launchpad™ SensorTag 套件
這款 TI LaunchPad™ SensorTag 套件可提供整合式環境和動作感測器、多頻無線連線和易於使用的軟體,適用於連線應用之原型設計。只要運用單一套件,開發人員就能輕鬆建立具備 Bluetooth® 低耗能、藍牙網狀網路、Zigbee、Thread 和 2.4GHz 與 Sub-1GHz 頻率的專利通訊協定連線應用,以提供靈活性。
這套全新產品之拓展以 TI LaunchPad 生態系統為基礎,提供完全封閉並以電池供電的套件,其設計旨在實現快速原型設計,協助 IoT 開發人員評估新產品構想,無需從頭開發任何硬體或軟體。有了這款可立即使用的硬體,開發人員即可 (...)
適用 SimpleLink™ 多頻帶無線 MCU 的 CC1352R LaunchPad™ 開發套件
CC1352R 多頻無線 MCU 是 SimpleLink™ 微控制器 (MCU) 平台的一部分,由 Wi-Fi®、Bluetooth® 低功耗、Sub-1 GHz、Thread、Zigbee®、802.15.4 與主機 MCU 組成,各系統共用一個配備單一核心軟體開發套件 (SDK) 與各種工具組的共同易用開發環境。SimpleLink 平台的一次性整合可讓您在設計中增加任何產品組合的裝置組合,且在設計需求改變時允許 100% 代碼重複使用。此 LaunchPad 套件支援 Code Composer Studio™ 及 IAR Embedded Workbench® 整合式開發環境 (...)
Technical Resources
mioty frequently asked questions (FAQ)
MIOTY, the new LPWAN standard, provides quality and scalability for worldwide Sub-
mioty modules with Radiocrafts
Find answers to common questions
How does the mioty technology compare to other LPWAN technologies?
Mioty is unique in the way it transmits data. Instead of sending it as one packet, mioty divides the telegram (data packet) into multiple sub-telegrams that are distributed in the time and frequency domains. This makes mioty more scalable and robust compared to other LPWAN technologies.
What kind of range can I expect from mioty?
5km in urban and 15km in rural environments.
What frequency bands are supported with mioty?
As described in the specification, the 868MHz and 915MHz frequencies are supported by the TS-UNB family.
What’s the timeline for support of bi-directional communication?
The mioty stack from Stackforce already has support for bi-directional communication as well as the gateways from the different gateway providers.
Where do I find information about the PHY and security features of mioty?
mioty is based on the telegram splitting ultra-narrow band (TS-UNB) family in the ETSI TS103358 standard. If you are interested in the technological details about the protocol, please refer to chapter 6 of the specification.
How does the licensing fee for mioty work?
There is an IP license cost related to using mioty, this is a one-time cost per device, which is handled by Sisvel. Refer to their website for more details.
What are the key differences between the high-performance gateway and the low-cost gateway? Are there any differences in scalability?
The main difference is in the dynamic range and in the linearity. This will affect the receives ability to handle weak signals in the presence of other stronger wanted and/or unwanted signal. This could potentially influence the scalability, but from a signal processing side, there should be no difference with regards to scalability. The low-cost gateway is mainly intended for evaluation use, for indoor deployment or for rural areas whereas the high-performance gateway should be used for outdoor urban solutions.
What gateways are currently on the market and what do they cost?
There are currently three mioty gateways on the market from Diehl, BehrTech and Weptech. Please visit the mioty store to see their offering and request a quote or contact the manufactures directly.