SOLUTION_ADAPTER

适用于 C2000™ MCU 的 powerSUITE 数字电源解决方案适配器工具

SOLUTION_ADAPTER

概述

The Solution Adapter is one of several tools included in the powerSUITE Digital Power Supply Design Software Tools for C2000™ Microcontrollers.  The Solution Adapter allows you to modify existing code examples from TI digital power kits and configure them to run on a custom digital power design.  The graphical interface steps you through the process of selecting the solution to adapt, selecting the relevant options for that solution (like device and control mode), and customizing the solution for your design.

To get started using the Solution Adapter:

  1. Follow the steps on the powerSUITE  page.
  2. Click on the Solution Adapter icon inside powerSUITE. All of the TI kits supported by the powerSUITE framework are displayed here. Select the solution you are interested in.
  3. On the next page, select the options for the solution, such as the device and the control mode, by clicking on the corresponding button.
  4. A dialog box will pop-up asking you to select the location to save the project.
    • Note: This location should reside outside of the controlSUITE file structure.
  5. A project will be created at this location for the solution selected and a GUI page from the project will appear inside CCS which will allow customization of the solution, for example changing the inductance value, changing the capacitance value, changing the build level, etc.
  6. For details on how to use the Solution Adapter with an existing TI development kit, you can refer to the user guide for the development kit and browse to the “Customize Solution Using powerSUITE” section.
  7. If you have questions, feel free to post them on the C2000 E2E Forum
特性
  • Graphical tool for creating digital control loop source code

  • The Solution Adapter Tool is included as part of powerSUITE

下载 观看带字幕的视频 视频

相关设计资源

硬件开发

子卡
BOOSTXL-BUCKCONV 数字电源降压转换器 BoosterPack

软件开发

驱动程序或库
CONTROLSUITE controlSUITE™ 软件套件:适用于 C2000™ 微控制器的软件和开发工具 SFRA 软件频率响应分析器 (SFRA)
IDE、配置、编译器或调试器
POWERSUITE powerSUITE

支持和培训

可获得 TI 工程师技术支持的 TI E2E™ 论坛

查看全部论坛主题 查看英文版全部论坛主题

所有内容均由 TI 和社区贡献者按“原样”提供,并不构成 TI 规范。请参阅使用条款

如果您对质量、包装或订购 TI 产品有疑问,请参阅 TI 支持

视频