Design Name C:/srf04/Agama/Agama_704k_EM_Designs/CC1352-P7EM-XD7793-XD24-PA24_10dBm/Cadence/allegro/CC1352-P7EM-XD7793-XD24-PA24_10dBm.brd
Date Tue Nov 24 10:52:55 2020
Note: This report identifies the unused B/B vias associated with a via stack structure. A stack structure can consist of coincidently placed micro, B/B vias or a combination. As an example of what the report detects, consider the stack Micro1-2, BB2-7, Micro7-8; if a trace connects to the stack on Layers 3 and 6, Micro1-2 and Micro7-8 would be identified as "unused". Click on the hyperlink to navigate to their location.
Unused Blind/Buried Vias
| Net Name |
Padstack Name |
Start/Stop Layer |
Location (x y) |