• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AWR6443Device Silicon ErrataSilicon Revision 2.0

    • SWRZ098 April   2021 AWR6443

       

  • CONTENTS
  • SEARCH
  • AWR6443Device Silicon ErrataSilicon Revision 2.0
  1. 1Introduction
  2. 2Device Nomenclature
  3. 3Device Markings
  4. 4Usage Notes
    1. 4.1 MSS: SPI Speed in 3-Wire Mode Usage Note
  5. 5Advisory to Silicon Variant / Revision Map
  6. 6Known Design Exceptions to Functional Specifications
    1.     MSS#25
    2.     MSS#26
    3.     MSS#27
    4.     MSS#28
    5.     MSS#29
    6.     MSS#30
    7.     MSS#31
    8.     MSS#32
    9.     MSS#33
    10.     MSS#36
    11.     MSS#37B
    12.     MSS#38A
    13.     MSS#39
    14.     MSS#40
    15.     MSS#41
    16.     MSS#43A
    17.     MSS#44
    18.     MSS#45
    19.     ANA#11A
    20.     ANA#12A
    21.     ANA#13B
    22.     ANA#14
    23.     ANA#15A
    24.     ANA#16
    25.     ANA#17A
    26.     ANA#18B
    27.     ANA#19
    28.     ANA#20
    29.     ANA#21A
    30.     ANA#22A
    31.     ANA#27A
  7. 7Trademarks
  8. 8Revision History
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

ERRATA

AWR6443Device Silicon ErrataSilicon Revision 2.0

1 Introduction

This document describes the known exceptions to the functional and performance specifications to TI CMOS Radar Devices (AWR6443).

2 Device Nomenclature

To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of Radar / mmWave sensor devices. Each of the Radar devices has one of the two prefixes: XAx or AWR6x (for example: AWR6443ABGABLRQ1). These prefixes represent evolutionary stages of product development from engineering prototypes (X6x) through fully qualified production devices (AWR6x).

Device development evolutionary flow:

XA — Experimental device that is not necessarily representative of the final device's electrical specifications and may not use production assembly flow.
AWR — Production version of the silicon die that is fully qualified.

XA devices are shipped with the following disclaimer:

"Developmental product is intended for internal evaluation purposes."

Texas Instruments recommends that these devices not to be used in any production system as their expected end –use failure rate is still undefined.

3 Device Markings

Figure 3-1 shows an example of the AWR6443 Radar Device's package symbolization.

GUID-FBD17B90-DCEE-47DF-A254-2B48E9400FD2-low.gif Figure 3-1 Example of Device Part Markings

This identifying number contains the following information:

  • Line 1: Device Number
  • Line 2: Safety Level and Security Grade
  • Line 3: Lot Trace Code
    • YM = Year/Month Code
    • Z- Assembly Site Code
    • LLL = Assembly Lot
    • S = Primary Site Code
  • Line 4:
    • 678A = AWR6443 (ES2.0) Identifier
    • ABL = Package Identifier
    • G1 = "Green" Package Build (must be underlined)

4 Usage Notes

Usage notes highlight and describe particular situations where the device's behavior may not match presumed or documented behavior. This may include behaviors that affect device performance or functional correctness. These usage notes will be incorporated into future documentation updates for the device (such as the device-specific data sheet), and the behaviors they describe will not be altered in future silicon revisions.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale