• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Why low-power mmWave radar is better than ultrasonic in parking assistance applications

    • SSZTD01 October   2023 AWRL1432

       

  • CONTENTS
  • SEARCH
  • Why low-power mmWave radar is better than ultrasonic in parking assistance applications
  1.   1
  2.   2
    1.     3
    2.     Where ultrasonic sensors are today
    3.     Advantages of using radar sensors for parking assistance
    4.     Conclusion
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Why low-power mmWave radar is better than ultrasonic in parking assistance applications

Jin Lee

Today’s parking systems primarily use ultrasonic sensors, a low-cost solution that can detect objects nearby. Although this technology is well-established, original equipment manufacturers (OEMs) must meet evolving requirements for parking assistance and autonomous parking applications in a cost-sensitive market, while tier-1 manufacturers see diminishing returns on their efforts to extract more performance from ultrasonic sensing.

The next generation of parking assistance, autonomous parking, and valet parking assist systems will all require detection of the vehicle’s surroundings with greater resolution, accuracy, and range than what is capable with ultrasonic sensing alone.

Where ultrasonic sensors are today

Ultrasonic parking systems vary in autonomy levels, from alerting drivers of detected objects to maneuvering the vehicle into parking spaces with the assistance of camera sensing. As shown in Figure 1, these systems use eight to 12 ultrasonic sensors positioned around the vehicle to achieve full coverage, with a typical detection range of 10 cm to 5 m.

GUID-0738BBB5-6216-471D-A46B-C8C0CD9E25B5-low.jpg Figure 1 Comparison of an ultrasonic sensor (left) and an AWRL1432 sensor (right) parking configuration

Ultrasonic sensors detect objects by emitting sound waves that are reflected by objects in its path. They measure the elapsed time between the emission of the sound wave and the reception of its echo to calculate the distance of nearby objects. Today, these sensors typically send the entire waveform of the received signal over high-speed Distributed System Interface (DSI3) channels to a central sensor fusion electronic control unit (ECU).

In contrast to ultrasonic sensors that emit sound waves, millimeter-wave (mmWave) radar sensors detect objects by emitting electromagnetic waves whose frequency increases over time. These signals reflect off of objects in a given pathway. The mmWave sensor measures changes in the properties of the detected objects to calculate their distance, velocity and angle of arrival.

77-GHz mmWave radar has steadily grown in popularity for both advanced driver assistance systems and body applications because of its wide radio frequency bandwidth, which enable precise range and velocity measurements. Despite its low cost, devices such as TI’s AWRL1432 single-chip radar sensor enable the accurate detection of objects in a range of 4 cm to 10 m and beyond, depending on antenna configuration. This extended range detects obstacles earlier, giving drivers more time to react and maneuver safely.

Advantages of using radar sensors for parking assistance

Ultrasonic sensors are optimized for the transmission of sound waves through one type of medium, such as air; thus, environmental conditions like mud, rain and fog can limit its performance. In contrast, the electromagnetic waves used by mmWave radar do not require a transmission medium, and can provide precise object detection under any external condition. Radar sensors are also generally less prone to false readings than ultrasonic sensors, offering a reliable solution for parking assistance functions.

Also, because ultrasonic sensors are affected by the mediums through which their sound waves propagate, installing an ultrasonic parking system in a vehicle involves a difficult process of drilling and painting holes in the bumper, incurring a significant cost to OEMs. In contrast, mmWave radar sensors can be mounted on the vehicle bumper as shown in Figure 2, simplifying installation while preserving aesthetics.

TI’s AWRL1432 mmWave radar sensor integrates the analog front end with a digital processing back end, enabling the transfer of processed output data over a cost-effective Controller Area Network Flexible Data-Rate channel for decision-making by the central ECU. The DSI3 cabling required to communicate waveform data from ultrasonic sensors to the central ECU is expensive in comparison. You can also use the AWRL1432 sensor in conjunction with existing corner radars on vehicles, which are becoming commonplace, allowing for multipurpose sensor reuse in an increasingly space-constrained sensing system.

GUID-91007ECF-9DE0-4817-AD37-63106BC46967-low.png Figure 2 A multimode corner radar system with the AWRL1432

Conclusion

The AWRL1432 sensor provides greater range, resolution and accuracy to help meet today’s requirements for not just parking assistance but entry-level blind-spot detection and higher-autonomy future applications such as valet parking. Its low-power architecture requires less active power and introduces idle and deep-sleep modes, offering the benefits of radar in kick-to-open and door-sensing applications that require battery power.

The AWRL1432 sensor not only enables OEMs and tier-1 manufacturers to improve radar performance in parking systems, but also enables implementation into exterior applications previously gated by cost and power. These features enable the development of software-defined, multipurpose radar that can reuse the same hardware and shorten engineering cycles across applications for the next generation of near-field sensing.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2024, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale