• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Capacitive Sensing: Simple Algorithm for Proximity Sensing

    • SSZTBV9 november   2015 FDC1004 , FDC2112 , FDC2114 , FDC2212 , FDC2214

       

  • CONTENTS
  • SEARCH
  • Capacitive Sensing: Simple Algorithm for Proximity Sensing
  1.   1
  2.   2
    1.     3
    2.     Derivative Integration Algorithm
    3.     IIR Filter Implementation
    4.     Summary
    5.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Capacitive Sensing: Simple Algorithm for Proximity Sensing

Rachel Liao

Proximity-sensing applications require the detection of small changes in capacitance (typically on the order of a few femtofarads) around the noise floor. Since there are many ways to process the data to determine whether a target was detected or not, how do you choose the best method? In this post, I’ll describe a simple algorithm that you can use for proximity sensing or capacitive touch applications that does not require significant processing overhead.

Derivative Integration Algorithm

A derivative integration algorithm (see the pseudo code shown in Figure 1) is a simple way to process the data. You can use it for both proximity sensing and capacitive touch buttons; the only difference between the two would be the derivative and integration thresholds for each sensor to obtain a robust and highly sensitive response.

GUID-BD38CA5E-7AD3-461C-B7DD-90A95AD92901-low.jpg Figure 1 Pseudo Code for the Derivative Integration Algorithm

This algorithm tracks the rate of change or derivative, D[i], between the current measurement, X[i], and the previous measurement, X[i-1]. Proximity-sensing applications require the detection of small capacitance changes. This requires the derivative threshold, DT, to be very low. Changes in capacitance due to noise can be a severe problem, especially if the DT is very low. The integral of the derivative, I[i], can start to accumulate and falsely trigger as a detected object. Random noise should stabilize the integral value so that the mean is zero (no capacitance drift occurs), but a high integration threshold, IT, can allow enough noise margin for nonrandom noise.

The leakage factor, L, is a value between 0 (instant dissipation) and 1 (no dissipation). It is typically set at 0.99 to represent that the algorithm has some memory of past values to determine where the detection boundary occurs. You can use various leakage factors for a faster recovery time if the integral swings too far positive. This will cause temporary sensitivity reduction until the integral can stabilize near 0.

Once a human hand approaches the sensing area, the integration value will start to accumulate as long as the derivative of the measurements hits the derivative threshold. If the device detects the hand (the integral value goes below the integration threshold) and the hand stops in the sensing area, the derivative flattens out and the integral stops accumulating. As the hand moves away from the sensor, the integral recedes until it goes above the integral threshold. This indicates that the target object is outside the intended sensing range.

For capacitive touch applications, a low derivative threshold is not required. You can optimize the integration threshold based on the desired button response. You can also implement multiple derivative and integration thresholds to filter out any high-frequency noise seen in the sampled measurements and increase the sensitivity response.

Figure 2 shows an example of a waveform with a target detected using the FDC2214. As the derivative becomes more negative (an object approaches the proximity sensor), the integral count matches the raw code signal, as expected. You can also optimize the thresholds to be robust against any slow-moving drift. Figure 3 shows how a drift in the raw code is compensated in the integral count. The signal is preserved without any distortions due to the slow upward drift.

GUID-9D44010B-29E6-405A-A307-E6DE4EE59DB8-low.png Figure 2 Example 1 – Proximity Raw Code, Derivative and Integral Waveforms
GUID-12D10E07-CCEF-4881-B34A-66C55355450B-low.png Figure 3 Example 2 – Raw Code and Integral Count

IIR Filter Implementation

To improve the signal-to-noise ratio in the measurements, you can implement an Infinite Impulse Response (IIR) filter to process the data and obtain an average measurement before sending it through the derivative integration algorithm. The IIR filter implementation is similar to a moving average except that previous values are not stored and shifted out of the summing order. This process saves memory and computational time at the expense of slight accuracy degradation.

The filter processes a running total of ‘N’ values. The current average (Avg[i]) is calculated by taking the previous average (Avg[i-1]), multiplying by N and subtracting the previous average. Then, the new value (val[i]) is added to the sum to create a “new sum”. Dividing by N creates a new average. Having N be multiples of two allows bit shifting instead of actually dividing, thus saving computational cycles.

Equation 1. GUID-07AB6AB4-CD6C-499E-920E-67B1BD2C36E0-low.png

Summary

The derivative integration algorithm is a simple algorithm that can be used to for proximity sensing and capacitive touch applications. This solution is a foundation that other sophisticated processing algorithms can be combined with to make the algorithm more robust for various system conditions. Depending on the system requirements, you will need to optimize the processing, but the derivation integration algorithm is a great start for quick prototyping.

Additional Resources

  • Find out more about TI’s capacitive-sensing portfolio.
  • Watch the capacitive sensing overview video.
  • Read the application note to learn more about the algorithm for proximity sensing.
  • Read other blog posts about capacitive sensing.
  • Share ideas with other engineers on the TI E2E™ Community Capacitive Sensing forum.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale