• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Eight Things to Consider When Choosing Haptic Feedback – Part 2

    • SSZTAZ3 August   2016 DRV2624 , DRV2625

       

  • CONTENTS
  • SEARCH
  • Eight Things to Consider When Choosing Haptic Feedback – Part 2
  1.   1
  2.   2
    1.     3
    2.     Closed-loop Architecture
    3.     Power Consumption
    4.     Integrated Haptics Library
    5.     Bonus: Controlling Your Driver
    6.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Eight Things to Consider When Choosing Haptic Feedback – Part 2

Kelly Griffin

GUID-3AC7F656-BA33-4E98-8628-C3847DBC0245-low.png

In the first installment of this two-part series, I discussed five things you should consider when picking a haptic driver and recent haptic advancements. To close this series off, we will cover the three remaining reasons.

Closed-loop Architecture

As in most systems, closed-loop architectures are the most ideal designs. TI’s closed-loop architecture provides several benefits for driving linear resonance actuators (LRAs) and eccentric rotating masses (ERMs).

ERMs are driven at DC voltage levels, so the resonance-tracking portion of the algorithm is not necessary. Instead, the DRV262x family takes advantage of other properties of the DC motor – mainly the attribute called back electromotive force (EMF). When an ERM is off, the motor produces current that is fed back to the outputs of the DRV262x. This current is used to determine how strong to push the motor for the next cycle. By measuring the back EMF, the DRV262x family reduces the power consumption needed to drive an ERM. Essentially, the TI haptic driver takes advantage of the momentum of the rotating mass and only provides the necessary push to keep the motor’s acceleration constant. This feature leads to power savings when compared to a discrete field effect transistor (FET) solutions.

As you may know, LRAs are high Q systems, meaning that they operate efficiently at a specific frequency. Figure 1 depicts the typical operating frequency of an LRA. Operating an LRA at a frequency just 2.5Hz outside of the resonance frequency can result in a 40% loss of acceleration. TI’s algorithm uses the properties of these LRAs to ensure that the drive frequency is within 2Hz of the actuator’s resonance frequency. The DRV262x can also accommodate a wide range of LRA frequencies from 45Hz to 300Hz. Just like the ERM, the back EMF is used to make sure we drive the LRA to its maximum potential with minimal effort.

GUID-0B4C17F6-1FAD-4279-AC5F-4950CCC59CCA-low.png Figure 1 LRA High Q System

Power Consumption

This next feature is arguably the most important feature of the DRV262x family: in shutdown mode, the driver consumes only 105nA. Power consumption for personal electronics, wearables and infotainment consoles is trending downward with technological advancements. Battery capacity continues to grow, but designers need to tackle power consumption from both sides. Since designers are trying to run haptic devices on less power, the TI haptic team is focusing on ultra-low power devices, such as the DRV2624 and DRV2625, which improves power consumption from the previous haptic driver by 10x.

One issue with keeping parts in shutdown mode is the wake-up time. For haptics, it is especially important to provide a fast response time. With the DRV262x haptic driver, users can wake up the part and implement a waveform in 1ms, making the response time miniscule.

Integrated Haptics Library

On a different note, some may not know where to start with haptic feedback; others may know exactly what they want. For those who aren’t sure where to start or are looking for a simple haptic implementation, the DRV2625 ships with a licensed implementation of Immersion’s TouchSense 2200 waveform library. This library contains 123 waveforms that can provide effects from single clicks to ramp-transition clicks for gaming applications or custom haptic feedback alerts. The DRV2625 has the option to implement as many as eight waveforms in a single sequence, and those sequences can be looped in numerous ways to create endless configurations.

For those with haptic experience who want to create custom effects, the DRV2624 ships with 2kB of programmable RAM to create custom effects geared toward video games, virtual reality or other applications. Using a microcontroller, products can have numerous haptic effects stored in a central library and loaded into RAM based on user experiences. This makes the DRV2624 extremely versatile.

Bonus: Controlling Your Driver

The future of integrated electronics will be heavily impacted by the ability to engage customers through the sense of touch. When looking for a place to start with the aforementioned drivers, consider using evaluation modules (EVMs), such as the DRV2625EVM-CT and DRV2624EVM-CT in conjunction with haptic control console (HCC). HCC is a program designed to make using haptic EVMs easy by utilizing an on board MSP430. This software controls every aspect of the DRV262x driver.

Now that you know what to look for when selecting a haptic driver, you should now be able to evaluate the different options and decide what is right for you. The haptic features for an automobile will be different than haptics in a smart watch or mobile device. There are certain features you should be on the lookout for, however.

Let me know what you think of these eight considerations. Would you add others?

Additional Resources

  • Visit the haptic portal for more information.
  • Read more blog posts on haptics.
  • Learn more about haptics in automotive, industrial, mobile and other applications from TI’s solution guides.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale