• Menu
  • Product
  • Email
  • PDF
  • Order now
  • IO-Link: the Backbone of the Smart Factory

    • SSZT956 september   2017 TIOL111 , TIOL1115 , TIOS101 , TIOS1015

       

  • CONTENTS
  • SEARCH
  • IO-Link: the Backbone of the Smart Factory
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

IO-Link: the Backbone of the Smart Factory

You’ve likely heard of the Internet of Things (IoT) and how it not only connects your internet-enabled devices to each other, but enables them to communicate and share data to improve your quality of life. Today, the manufacturing industry is using the IoT as a key piece of the next wave of manufacturing. Industry 4.0, which is a word some have coined to mean the next industrial revolution, describes factory automation and the ability to construct a “smart factory” where data is easily exchanged and harnessed to keep factories running at maximum efficiency. IO-Link is an important interface to implement this factory transition.

You may think that factories are already efficient based on the quality of products you buy today and the price at which you can purchase them. In reality, factories have numerous inefficiencies that an interface like IO-Link can help reduce. The IO-Link Consortium and International Electrotechnical Commission (IEC) 61131-9 standard established a bidirectional, manufacturer-independent communication protocol for sensors and actuators. The specification also defines a mechanical interface that is fully backward-compatible with existing field buses, such as Profibus, Profinet and EtherCAT, used today.

Let’s look at few key advantages of IO-Link and how they are helping drive factory automation:

  • Bidirectional communication. Today’s factories primarily use one-way sensors, meaning that they only provide data based on standard input/output (SIO)/digital output switches. So if a red wagon in a toy factory comes down the line painted green, the one-way sensor alerts engineers of the fault. But that isn’t helpful if someone actually ordered a green wagon. IO-Link’s bidirectional protocol enables factories to easily update sensor parameters, enabling custom orders without going to the factory floor to reprogram each sensor. Bidirectional communication also provides factories real-time information about cable breaks, overtemperature conditions, output shorts and transfer diagnostics. In some cases, the sensor can even alert the factory that it is nearing its end of life.
  • Manufacturer-independent. Manufacturers who follow the IO-Link standard will produce sensors and actuators that operate, not only with their other products (sensors, programmable logic controllers [PLCs]), but with competitor solutions. A standard interface, cable and connector gives factories the ability to develop a process that delivers products based on their key requirements, while maintaining a high level of efficiency and flexibility.
  • Communication protocol. IO-Link’s point-to-point communication protocol enables up to 32 bytes depending on the required cycle time. Additionally, the IO-Link master can store sensor and timing parameters. This key feature enables engineers to easily switch out faulty sensors and download parameters to the new sensor automatically, further reducing downtime and increasing factory efficiency.
    • Backward compatibility. As I mentioned, SIO/digital output switches are the primary interface to the PLC today. There are many SIO sensors installed in factories today, and the thought of replacing them with a new technology is an overwhelming one. The IO-Link authors recognized this and mandated that the connector for IO-Link must use not only the same connector/pinout as the installed base, but also the same cabling, so that manufacturers could easily update their factory lines.

These connectors, as shown in Figure 1, are based on the specifications outlined in IEC 61131-9. They are the same (M5, M8 and M12 type) connectors used throughout installations today.

GUID-28A7B3D7-43C8-4AFC-B5A4-164DD4CA8FB2-low.png Figure 1 IO-Link SIO Connectors

Connections can occur across a three-wire (or more) cable stretching to a maximum of 20 meters (66 feet). Table 1 defines the IO-Link signals.

GUID-67346DA4-2E6C-4CAF-B9C4-2FBF0050EE73-low.png

* Required for three-wire interface Table 1: IO-Link cable definitions

If you’re familiar with SIO, you’ll notice that its functions are the same as those listed in the table, with VCC, OUT and GND usually referenced. Both IO-Link and SIO use the C/Q (or OUT) signal for data.

TI has shipped IO-Link-enabled transceivers since 2011 and recently released its second generation of transceivers. In my next blog post, I’ll talk about how our TIOL111 IO-Link device transceiver and TIOS101 digital output switch further enable smart factories.

Additional Resources

  • Learn more about our IO-Link and digital output switches.
  • Evaluate your device today with the TIOL1115 and TIOS1015 evaluation modules.
  • Download the Smart Solenoid Driver with Predictive Maintenance Reference Design featuring the TIOL111.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale