• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Pull the Tab: How to Implement Ship Mode in Your Lithium-ion Battery Design

    • SSZT534 february   2019 BQ21061 , BQ21062 , BQ25120A , BQ25122 , BQ25125 , BQ25150 , BQ25155

       

  • CONTENTS
  • SEARCH
  • Pull the Tab: How to Implement Ship Mode in Your Lithium-ion Battery Design
  1.   1
  2.   2
    1.     3
    2.     What Is Ship Mode, and Why Do You Need It?
    3.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Pull the Tab: How to Implement Ship Mode in Your Lithium-ion Battery Design

Gautham Ramachandran

Remember when you were a kid and many of your battery-operated toys had a little plastic pull tab on the battery (Figure 1) that you pulled off to make the product come to life? This closes the connection from battery to the active circuit on the product and is one of the earliest implementations of “ship mode.”

In this blog post, I will address what ship mode is, and how you can use this feature in your product to deliver the best user experience. While I will be using TI battery charge management integrated circuits as examples, you can apply these concepts to any low-power system under development.

GUID-2BBA752A-0632-4EBF-8F5E-72DCA010BB73-low.jpg Figure 1 Pull Tab on a Battery-Operated Product

What Is Ship Mode, and Why Do You Need It?

Ship mode is the state in which the product is consuming the lowest battery current. Consumers naturally want to use battery-operated products immediately after purchasing them. This means that the battery has to maintain some capacity during transportation from the factory and during its shelf life, which could be a couple of months or even longer.

Lithium-ion batteries have become a popular choice for designers because they are rechargeable, support high-power requirements and are very light. However, unlike non-rechargeable batteries, you can’t put plastic tabs on products using lithium-ion batteries as you want to restrict access to these batteries for safety concerns. This means that we need to find alternative solutions for implementing the ship-mode feature for products both in its on and off states.

You might be wondering why you should care about ship mode when “shipping” happens only once, but that’s not exactly true. Ship mode is the state in which the product is consuming the lowest quiescent current, while waiting for the user to press a button to turn the product ON. For instance, TI’s BQ25120A is actively monitoring for either an adapter to be plugged in or a button-press input, all while consuming a typical current of 2 nA.

I often recommend that designers implement ship mode when the product is about to be boxed at the factory, is being used and running low on battery, and is being used and the user wants to power off the product.

The ship mode on the BQ25120A family of chargers is realized using a push-button interface, as shown in Figure 2. The push-button input (/MR) is internally pulled up to the VBAT pin. When the device is in ship mode and the user presses the /MR button, the product comes out of ship mode.

You don’t need a capacitor on this pin, as the signal is internally deglitched, but it is common to see them on some schematics. You could optionally use a transient voltage suppression diode for protection if the switch is exposed to the user. A low-voltage read on the /MR pin translates to a “button pushed” action. Take care when connecting to a microcontroller (MCU) to drive the /MR pin, as voltage on the /MR pin is pulled to the battery voltage itself. An N-channel metal-oxide semiconductor is often employedto mimic a “press” action from the MCU in a buttonless system.

GUID-DBF235CF-9560-4EE9-9443-7E314F0E2A09-low.png Figure 2 Internal Pullup on the /MR Pin

When a product is about to be boxed at the factory, the EN_SHIPMODE command is sent over I2C and the device waits to go to ship mode until the VIN(charger) is disconnected, as shown in Figure 3.

GUID-AAEBE7A4-1B2C-413F-A90A-29F9574269DF-low.png Figure 3 Illustration of Ship Mode at a Factory Production Line

I have seen many challenges on the production line. Things work great in the lab, but on a line that’s building a few hundred products an hour, it can be a different story. The product is on a jig and the assembler doesn’t have a proper way to pull off the product without the VINadapter bouncing. The charger will get out of ship mode when VINlooks like it was plugged back in. How do you make sure that the product is in ship mode in this case?

The answer is simple: Set the EN_SHIPMODE command when the VINis present. Once the product is off the jig that supplied the VIN, raise the /CD pin high to complete the execution of the ship-mode command and put the device to a ship mode before being boxed, as shown in Figure 4. In all these sequences /MR is being pushed to show that the device has indeed gone into ship mode.

GUID-5B5F680A-AC45-4BAF-B82E-E58EE419CC4D-low.png Figure 4 Illustration of Ship Mode at a Factory with a Bouncy Adapter

When the product is running low on battery, often the best way to power down is to keep some reserve capacity and then go into ship mode. When the user presses the button, the device can read the battery level. If the battery level is too low, the product can display a warning and return back to ship mode, as shown in Figure 5. When using the BQ25120A, for example, you can send the ship-mode command using a single register write as shown in Figure 6.

GUID-C491513A-6973-4284-99FC-EE853AFF3A4E-low.png Figure 5 Wake-Up Routine for your Product
GUID-3C18F5A1-191D-4D5C-B045-BAA79D3165B1-low.png Figure 6 Ship Mode Entry through I2C Command

Also, to create a power on/off button, you could still use the /MR pin by configuring the MRREC register to go to ship mode and programming the duration of the button of how long it needs to be held low; you’ve just created yourself a power-off button. To wake back up, press the button again, as illustrated in Figure 7.

GUID-A7B332D9-F85C-488D-8CEE-37B020A57FA7-low.png Figure 7 Power On/Off Button

I hope that this post has given you a good idea on how to use some of the features that are present on a charger and ready to implement ship mode in your next product! Visit our E2E forums for any questions you might have.

Additional Resources

  • Download the BQ25120A data sheet.
 

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale