• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Integrating Multiple Functions within a Housekeeping MSP430 Microcontroller

    • SSZT248 october   2020 MSP430FR2000 , MSP430FR2100 , MSP430FR2110 , MSP430FR2111 , MSP430FR2422 , MSP430FR2433

       

  • CONTENTS
  • SEARCH
  • Integrating Multiple Functions within a Housekeeping MSP430 Microcontroller
  1.   1
  2.   2
    1.     3
    2.     Sample application: Implementing ADC wake and transmit functions on a housekeeping MCU
    3.     Conclusion
    4.     Additional resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Integrating Multiple Functions within a Housekeeping MSP430 Microcontroller

Shreya Mandal

You’re probably constantly looking for ways to optimize your printed circuit board (PCB) designs. From reducing board size to lowering costs and component count, maximizing efficiency is a requirement for almost any design.

Adding a small, low-cost microcontroller (MCU) for simple housekeeping functions can benefit many board designs. This housekeeping (or secondary) MCU is not the main host processor in the system, but it can handle several important system-level functions such as LED control or input/output (I/O) expansion. In this article, I’ll explain how integrating a multifunction housekeeping MCU in your system can help lower bill-of-materials (BOM) costs, save board space, and best of all simplify your design.

For example, let’s say that you wanted to create a new design with these features:

  • LED control
  • I/O expansion
  • External electrically erasable programmable read-only memory (EEPROM)
  • An external watchdog timer

It is possible to use discrete integrated circuits (ICs) to achieve each of these functions. Instead, consider performing all of the functions in software on a housekeeping MCU in order to minimize complexity and reduce board size, as shown in Figure 1.

GUID-6BBE9AE5-4236-43E1-970F-1607C4506BE9-low.jpg Figure 1 Implementing the functionality of multiple discrete ICs and in software on a single housekeeping MSP430 MCU

Another design challenge to consider – and perhaps one of the most important – is meeting your design budget.

For instance, looking at the costs associated with a discrete IC approach for these features, you could expect these approximate BOM costs (using web pricing):

  • LED controller IC: approximately $0.20
  • Five-channel I/O expander IC: approximately $0.25
  • Serial EEPROM (4KB): approximately $0.20
  • External watchdog timer: approximately $0.315

In total, a discrete approach to handle housekeeping functions would cost around $0.97. Compare that to the current web price for an 8KB MSP430 MCU, which is less than $0.25. That’s quite a large savings!

If you require more or less memory for your housekeeping MCU, you can find various options that scale across memory and price in the MSP430 MCU portfolio. Table 1 lists these MCUs and their current TI.com pricing.

Table 1 Housekeeping MSP430 MCUs with TI.com pricing
Memory Product Pricing
0.5KB MSP430FR2000 See Pricing
1KB MSP430FR2100 See Pricing
2KB MSP430FR2110 See Pricing
4KB MSP430FR2111 See Pricing
8KB MSP430FR2422 See Pricing
16KB MSP430FR2433 See Pricing

Not only does an integrated housekeeping MCU approach save board size and reduce the number of components, it also saves BOM costs. You can learn more about these design considerations in the webinar, “Simpler system monitoring: How to offload multiple functions to an MSP430 MCU.”

Sample application: Implementing ADC wake and transmit functions on a housekeeping MCU

Let’s walk through an example of how to actually implement the housekeeping function within your design.

One common function is an analog-to-digital converter (ADC) interfacing with other devices on a board for applications such as battery monitors or temperature sensors. In this example, the ADC must periodically sample the analog signals from the sensors and send this data back to the MCU, which will take action based on the behavior of those signals.

If the MCU is using timers to trigger ADC reads, or even receiving ADC values continuously, the system can consume quite a bit of power. One solution is to integrate the ADC into the MCU and operate it independently of the central processing unit (CPU). That way, the rest of the MCU can go to sleep and will only wake up when the ADC reads a value that crosses a certain threshold. At this point, the ADC will generate an interrupt and wake up the MCU.

We describe this application in our training video about housekeeping functions, “ADC Wake and Transmit on Threshold Using MSP430 MCUs.” In this video, we show a graphical user interface (GUI) demonstrating the reading of the ADC values and the sending of the interrupt to wake up the CPU once the threshold is met.

ADC Wake and Transmit on Threshold

Conclusion

Using another MCU to perform housekeeping functions is a great way to simplify your design. Plus, with our software and GUI, you can program your MSP430 device in minutes to handle a variety of functions.

Additional resources

  • Learn more about the ADC wake and transmit function in the application note, “ADC Wake and Transmit on Threshold Using MSP430 MCUs"
  • Try the ADC wake and transmit software example on an MSP430FR2433 LaunchPad™ development kit.
  • Watch our training video “ADC Wake and Transmit on Threshold with a Housekeeping MCU”
  • Download and test this example with the ADC Wake and Transmit demo GUI

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale