SPRADN2 January 2025 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3519 , MSPM0L1227 , MSPM0L1228 , MSPM0L2227 , MSPM0L2228
With the growing demand of applications such as automotive systems which have strict real-time needs, accessing critical information about the system functionality is necessary before the completion of a Flash memory erase or program operation. Applications need a firmware upgrade, especially when the system power loss occurs during the update process. This can result in many problems such as a transmission error or an information loss. For these reasons, TI offers MSPM0 MCUs that embed dual bank Flash memories designed to respond to the above needs. The dual bank Flash memory allows a code to be executed in one bank, while another bank is being erased or programmed. This avoids a CPU stalling during programming operations and protects the system from power failures or other errors. This application note gives an overview of the MSPM0L, MSPM0G Series Flash memory dual bank capabilities, and shows how to implement Bank Swap function on customer project.
All trademarks are the property of their respective owners.
The nonvolatile memory system provides on-chip programmable flash memory for storing executable code and data, the device boot configuration, and parameters which are preprogrammed by TI from the factory. The NVM is organized into one or more banks, and the memory in each bank is further mapped into one or more logical memory regions and system address space for use by the application. Key flash bank terms are defined in Table 1-3 to be used as a reference for the rest of this application note.
Term | Definition | Size |
---|---|---|
Flash word | Basic data size for program and read operations on the flash memory (also the read bus width to the system) | 64 data bits (72 bits with ECC) |
Word line | Group of flash words within a sector, with maximum program operation limit before sector erase | 16 flash words (128 data bytes, optionally 16 ECC bytes) |
Sector | Group of word lines that are erased together (minimum erase resolution of the flash memory) | 8 word lines (1024 data bytes, optionally 128 ECC bytes) |
Bank | Group of sectors that can be mass erased in one operation. Only one read, program, erase, or verify operation can run concurrently on a given bank. | Variable |
The NVM system on MSPM0 device provides support for up to 5 flash memory banks (enumerated as BANK0 through BANK4). The number of flash banks present is device dependent. To determine the bank scheme of a particular device, review the detailed description section of the specific device data sheet Flash Memory chapter.
Within a given flash bank, an ongoing program or erase operation stalls all read requests to that bank until the operation has completed and the flash controller has released control of the bank. On devices with more than one flash bank, read request to other flash banks are unaffected by operations in a different flash bank. As such, the presence of multiple banks improves performance in application cases such as:
Flash Memory Region | Region Contents | Executable | Used by | Programmed by |
---|---|---|---|---|
FACTORY | Device ID and other parameters | No | Application | TI only (not modifiable) |
NONMAIN (Configuration NVM) | Device boot configuration (BCR and BSL) | No | Boot ROM | TI, User |
MAIN (Flash Memory) | Application code and data | Yes | Application | User |
Devices with one bank implement the FACTORY, NONMAIN, and MAIN regions on BANK0 (the only bank present), and the DATA bank is not available. Devices with multiple banks also implement FACTORY, NONMAIN, and MAIN regions on BANK0, but include additional banks (BANK1 through BANK4) that can implement MAIN or DATA bank.
Operating on a NVM
Any interruption during the erase or re-program operations (that is, unplugging device, removing SWD jumpers, hitting reset by accident, canceling the code download, an IDE crash, and so forth) can brick the device permanently. Improper configuration of NONMAIN can also lead to permanent locking of the device.
Figure 1-2 is an example of a three bank configuration with a 512KB MAIN region split across BANK0 and BANK1, with a 16KB DATA bank provided in BANK2. Like the single bank example, NONMAIN and FACTORY regions are included in BANK0. This example supports EEPROM emulation in the DATA bank without stalling fetches to MAIN, and also supports dual-image applications where BANK0 main can be written to without stalling fetches to BANK1 main (and the reverse). Most devices with a main region ≥256KB in size implement some form of multibank configuration.
For multi bank devices, the BANK0 and BANK1 are considered as Physical Bank 0 (PB0) and Physical Bank 1 (PB1). These banks can switch addresses depending on the bank swap configuration, but upon a BOOTRST the entry point is always PB0.
For example, the Logical Bank 0 (LB0) always maps to address 0x0000.0000 - 0x0003.FFFF, and Logical Bank 1 (LB1) maps to 0x0004.0000 - 0x0007.FFFF. The two logical banks can map to either PB0 or PB1.
Further sections focus on how to take advantage of multiple banks features to achieve application requirements.