SPRAD47 August 2022 TMS320F28379D
Sufficient stack memory space is an important factor for stable system operation. However, too large stack size allocation wastes the memory space and too small stack causes a system crash due to stack overflow. The allocation of the stack memory size has always been a matter of discussion. This application brief discusses how to monitor the used stack size at runtime for C2000™ real-time microcontrollers, and helps us to determine the optimal stack memory size.
The method typically used is to fill the stack with a known value (0xAA55) prior to running the code. During software development stage, you can use the fill command in the linker command file or use the Code Composer Studio™ (CCS) memory fill option to fill the entire stack with the defined known value. Then, when you run the application code, anytime you halt you can use the CCS memory browser to check the stack memory to see how much stack space has been used.
However, if you want to monitor the stack utilization in standalone mode, or generate a hex file for firmware upgrade or a standalone programmer, you should not use the fill command in the linker command file. Instead you need a method to fill the stack at runtime and to monitor the stack utilization. To achieve this, the below proposed _system_pre_init() function can be a good method.
The _system_pre_init() function is invoked after the stack pointer is initialized and before any C/C++ environment setup is performed. To keep the used stack memory size under control, create the small piece of C code in the application software filling the stack space.
Add the C code shown below to your application software, so that you are able to obtain the stack space size and start address information: either legacy COFF or EABI format.
01 #if defined(__TI_EABI__)
02 #define STACK_MEM_ADDR __stack // Symbol of stack start address
03 #define STACK_MEM_SIZE __TI_STACK_SIZE // Symbol of stack memory size
04 #else
05 #define STACK_MEM_ADDR _stack // Symbol of stack start address
06 #define STACK_MEM_SIZE _STACK_SIZE // Symbol of stack memory size
07 #endif
08
09 #define STACK_KNOWN_DATA 0xAA55 // Define the known data
10
11 extern int *STACK_MEM_ADDR;
12 extern void *STACK_MEM_SIZE;
Include the C function shown below to fill the stack space with the defined known data at runtime. When caller calls this function, the Return Program Counter (RPC) register value is pushed on the stack, then the function return address is stored in the RPC register.
If a break point is set at line 10 of the _system_pre_init() function to halt, use the CCS memory browser to check stack space. You can see six words of stack space are used. Table 1-1 shows us the stack memory address description. Skip these used memories and fill the rest of stack space.
01 //
02 // Function used to runtime fill stack space with the known data
03 //
04 int _system_pre_init()
05 {
06 int *ptr_stack = (int *)(&STACK_MEM_ADDR); // Get stack start address
07 long stack_size = (long)(void *)(&STACK_MEM_SIZE); // Get stack memory size
08
09 // Skip used stack space
10 ptr_stack += 6;
11 stack_size -= 6;
12
13 // Fill unused stack space with the known data
14 do
15 {
16 *ptr_stack++ = STACK_KNOWN_DATA;
17 } while(--stack_size > 0);
18
19 // return one non-zero value
20 return 1;
21 }
| Stack Memory Address | Memory Description |
|---|---|
| Stack Start Address + 0 | RPC register data, 2 words |
| Stack Start Address + 2 | Local variable stack_size, 2 words |
| Stack Start Address + 4 | Local variable ptr_stack, 2 words |
| Stack Start Address + 6 to Stack Start Address + Stack Size - 1 |
Unused memory space |
Include the C code shown below to the application code, and periodically call the monitor_used_stack_size() function. For example, in the main routine or timer ISR, the global variable stack_mem_used shows the actual used stack size of the system.
When the system is operating in standalone mode, you can transmit this data to the terminal via the SCI port and then you can determine the maximum stack size needed for the system under all operating conditions. This information helps to optimize the stack size.
In this document, LAUNCHXL-F28379D is used to evaluate all the example C code. However, this runtime stack size monitoring example can be applied to all C28x C2000 devices.
01 // Global variable to monitor used stack size
02 long stack_mem_used = 0;
03
04 //
05 // Function to monitor used stack size
06 //
07 void monitor_used_stack_size(void)
08 {
09 int *ptr_stack = (int *)(&STACK_MEM_ADDR); // Get stack start address
10 long stack_size = (long)(void *)(&STACK_MEM_SIZE); // Get stack memory size
11
12 // Check the filled known data and determine used stack size
13 do
14 {
15 if(*ptr_stack++ == STACK_KNOWN_DATA)
16 {
17 break;
18 }
19 } while(--stack_size > 0);
20
21 // Get used stack size
22 stack_mem_used = ((long)(void *)(&STACK_MEM_SIZE) - stack_size);
23 }
This application document focuses on the application level, showing how to include the simple C code to fill stack memory with the known values at runtime, to monitor the amount of stack size required by the application code.
C2000 devices built-in the C28x Emulation Analysis Block that can be an alternate way to check the stack size needed by the application code. For details, see Online Stack Overflow Detection on the TMS320C28x DSP.