SPNA233B May 2016 – February 2020 RM41L232 , RM41L232 , RM42L432 , RM42L432 , RM44L520 , RM44L520 , RM44L920 , RM44L920 , RM46L430 , RM46L430 , RM46L440 , RM46L440 , RM46L450 , RM46L450 , RM46L830 , RM46L830 , RM46L840 , RM46L840 , RM46L850 , RM46L850 , RM46L852 , RM46L852 , RM48L530 , RM48L530 , RM48L540 , RM48L540 , RM48L730 , RM48L730 , RM48L740 , RM48L740 , RM48L940 , RM48L940 , RM48L950 , RM48L950 , RM48L952 , RM48L952 , RM57L843 , RM57L843 , TMS570LC4357 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LC4357-SEP , TMS570LS0232 , TMS570LS0232 , TMS570LS0332 , TMS570LS0332 , TMS570LS0432 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0714-S , TMS570LS0914 , TMS570LS0914 , TMS570LS1114 , TMS570LS1114 , TMS570LS1115 , TMS570LS1115 , TMS570LS1224 , TMS570LS1224 , TMS570LS1225 , TMS570LS1225 , TMS570LS1227 , TMS570LS1227 , TMS570LS2124 , TMS570LS2124 , TMS570LS2125 , TMS570LS2125 , TMS570LS2134 , TMS570LS2134 , TMS570LS2135 , TMS570LS2135 , TMS570LS2135-S , TMS570LS2135-S , TMS570LS3134 , TMS570LS3134 , TMS570LS3135 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137
This application report provides software source code and additional information on how to implement a workaround that helps to minimize the impact of Hercules Phase Locked Loop (PLL) Advisory SSWF021#45.
Project collateral and source code mentioned in this document can be downloaded from the following URL: http://www.ti.com/lit/zip/spna233.
All other trademarks are the property of their respective owners.
Texas Instruments has found that on rare occasions some Hercules Safety Microcontrollers have an issue with PLL startup. While Texas Instruments does test for and screen these devices, at the time of publication of this report, our screens are not 100% effective. Parts that are affected have advisory SSWF021#45 listed in the errata document for that device, if the errata document was published in May of 2016 or later. The software workaround described in this report, while not 100% effective, significantly helps to reduce the occurrence of failures.
The header file “errata_SSWF021_45.h” contains the function prototypes and should be included in the user’s source file that calls the workaround function. The header file “errata_SSWF021_45_defs.h” defines values used in the “errata_SSWF021.c” file. It makes the source file independent of HALCoGen.
NOTE
The workaround functions do not set the PLL to the customer's desired frequency, nor do they leave the PLL enabled. These steps should be performed after successful completion of the workaround routine. The PLL settings in the workaround routine were chosen to minimize the lock time and to be valid over the range of 5 MHz to 20 MHz crystal frequency. Changing these settings may affect the proper execution of the workaround routine.