SPMA082 August 2021 TM4C1230C3PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PZ , TM4C123BH6ZRB , TM4C123FE6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD
TivaWare is a trademark of Texas Instruments.
TrueType, OpenType, PostScript, and Windows are registered trademarks of Apple Inc., registered in the United States and other countries.
All trademarks are the property of their respective owners.
Thin Film Transistor (TFT) is a variant of LCD that uses TFT technology to improve image qualities. A TFT is an active matrix LCD, in contrast to passive matrix LCD or direct-driven LCD such as the character-based LCD with a few segments. The TFT LCD is a popular display type for small-to-medium size applications.
A typical TFT LCD module will consist of a TFT LCD panel, a chip-on-glass (COG) driver IC, a backlight unit, and an interface Flexible Printed Circuit (FPC). The TFT driver ICs are highly integrated chips that will combine the source driver (in a 320 x 240 display, driving 320 x 3 = 960 sources of the transistors for supporting Red, Green and Blue), gate driver (driving the 240 gates of the transistors), timing control and sometimes other circuits such as memory, power or image processing. The FPC provides an interface connector to the MCUs. Figure 1-1 shows the Kentec320 x 240 display that is mounted on the DK-TM4C129X EVM board shown in Figure 1-2. The driver IC on the Kentec320x240x16 is a SSD2119.
Depending on the particular TFT panel size and resolution, some driver ICs may support multiple interfaces to communicate with the host controller. The interfaces are normally selectable on the module FPC or through firmware initialization.
The LCD frame buffer is a contiguous memory block, storing enough data to fill a full LCD screen. The frame buffer contains the palette look-up table (palette RAM) and the frame data for a given source image. Operating in RGB Mode requires the LCD frame buffer. The LCD controller has the option to use the internal SRAM memory or external memory through the EPI interface to hold the frame buffer.