• Menu
  • Product
  • Email
  • PDF
  • Order now
  • LM61495RPHEVM EVM User’s Guide

    • SNVU682A July   2019  – March 2021 LM61495-Q1

       

  • CONTENTS
  • SEARCH
  • LM61495RPHEVM EVM User’s Guide
  1.   Trademarks
  2. 1Introduction
    1. 1.1 LM61495RPHEVM Synchronous Step-Down Voltage Converter
  3. 2Quick Start
  4. 3Detailed Descriptions
  5. 4Schematic
  6. 5Board Layout
  7. 6Board Curves
  8. 7Bill of Materials
  9.   Revision History
  10. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

EVM USER'S GUIDE

LM61495RPHEVM EVM User’s Guide

Trademarks

HotRod is a trademark of Texas Instruments Incorporated.

All trademarks are the property of their respective owners.

1 Introduction

1.1 LM61495RPHEVM Synchronous Step-Down Voltage Converter

The LM61495-Q1 is an easy-to-use synchronous step-down DC-DC converter capable of driving up to 10 A of load current from a supply voltage ranging from 3 V to 36 V. The LM61495-Q1 provides exceptional efficiency and output accuracy in a very small solution size. The LM61495-Q1 implements peak-current-mode control. Additional features such as adjustable/synchronizable switching frequency, pin selectable dual-random spread spectrum (DRSS), true slew rate control, FPWM/AUTO selection, power-good/RESET flag, and precision enable provide both flexible and easy-to-use solutions for a wide range of applications. Automatic frequency foldback (AUTO mode) at light load and optional external bias improve efficiency over the entire load range. The device family requires few external components and has a pinout designed for simple PCB layout with excellent EMI and thermal performance. Protection features include thermal shutdown, input undervoltage lockout, cycle-by-cycle current limiting, and hiccup short-circuit protection. The LM61495-Q1 is pin-to-pin compatible with LM62460-Q1 and LM61480-Q1 for easy current scaling.

The pin configuration of the LM61495-Q1 is shown in Figure 1-1.

GUID-C96249BE-2F32-4AF0-BA13-B21E78FE1773-low.gifFigure 1-1 LM61495-Q1 Pin Configuration (16-Pin VQFN-HR Package Top View)

2 Quick Start

  1. Connect the voltage supply between VIN_EMI and GND_EMI terminals using short, thick wires.
  2. Connect the load of the converter between VOUT and GND (J2) terminals, using short, thick wires.
  3. Set the supply voltage (VIN) at an appropriate level between 6 V to 36 V. Set the current limit of the supply to an appropriate level depending on the connected load.
  4. Turn on the power supply. With the default configuration, the EVM should power up and provide VOUT = 5 V.
  5. Monitor the output voltage. The maximum rated load current is 10 A.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale