• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Radiation Tolerant Inverting Buck-Boost Converter with TPS7H4010-SEP

    • SNVAA76 june   2023 TPS7H4010-SEP

       

  • CONTENTS
  • SEARCH
  • Radiation Tolerant Inverting Buck-Boost Converter with TPS7H4010-SEP
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Design Description
    2. 1.2 Design Goals
  5. 2Detailed Design Procedure
  6. 3Testing Results
  7. 4Summary
  8. 5References
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Application Note

Radiation Tolerant Inverting Buck-Boost Converter with TPS7H4010-SEP

Abstract

One common design challenge for space applications is the need to generate a negative voltage rail. This application note illustrates how to design an inverting buck-boost using the radiation tolerant TPS7H4010-SEP. Radiation tolerant devices are needed to shield against single event effects and dose effects in LEO™ applications. The TPS7H4010-SEP is rated for 30-krad (Si) for total ionizing dose and 43 MeV*cm2/mg for singe event latch-up immunity. This topology takes a positive input voltage and create a regulated negative output voltage. This application note details design considerations and simulation results, so that designers can scale the design to different requirements. The document also includes experimental results and configuration instructions to regulate voltage rails of -12 V, -6 V, and -1.8 V from a 12-V input and a 5-V input for the -6 V and -1.8 V rails.

Trademarks

LEO™ is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale