• Menu
  • Product
  • Email
  • PDF
  • Order now
  • LMR12010 Step-Down Converter Evaluation Module User's Guide

    • SNVA490B September   2011  – December 2021 LMR12010

       

  • CONTENTS
  • SEARCH
  • LMR12010 Step-Down Converter Evaluation Module User's Guide
  1.   Trademarks
  2. 1Introduction
  3. 2Features
  4. 3Enable Operation
  5. 4Adjusting the Output Voltage
  6. 5Test Setup
  7. 6Typical Performance Characteristics
  8. 7Layout
  9. 8Additional Circuit Configuration Schematics
  10. 9Revision History
  11. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

LMR12010 Step-Down Converter Evaluation Module User's Guide

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The LMR12010 is a step down DC-DC regulator that operates at the following switching frequencies: the LMR12010X at 1.6 MHz and the LMR12010Y at 3 MHz. The demo board is configured to convert 5-V input to 1.8-V output at 1-A load current using the Y version. The tiny low profile thin SOT23 package allows the design to use less than 1 square inch of board area.

The circuit is configured with the boost diode connected to VIN. VIN must not exceed the maximum operating limit of 5.5 V + VfD2 using this configuration. This makes sure that the voltage between the boost and SW pins, VBOOST – VSW, does not exceed 5.5 V for proper operation. For more information regarding this requirement, see the LMR12010 SIMPLE SWITCHER® 20Vin, 1A Step-Down Voltage Regulator in SOT-23 Data Sheet.

The schematics at the end of this document show how to reconfigure this demo board for various input and output conditions as discussed in the LMR12010 SIMPLE SWITCHER® 20Vin, 1A Step-Down Voltage Regulator in SOT-23 Data Sheet. Short or leave open the connections as indicated in the schematics. The previously mentioned restrictions for the input voltage are valid only for the demo board as shipped with the demo board schematic shown in Figure 4-3

2 Features

  • 3.0-V to 5-V input voltage range (as shipped)
  • 1.8-V output voltage
  • Up to 1-A output current
  • Switching frequency of 3 MHz
  • Small solution size (17 mm × 17 mm)

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale