• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Overvoltage Protection with Comparator Circuit

    • SNOAA20 January   2019 TLV1805 , TLV1805-Q1

       

  • CONTENTS
  • SEARCH
  • Overvoltage Protection with Comparator Circuit
  1.   1
  2.   2
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Analog Engineer's Circuit

Overvoltage Protection with Comparator Circuit

Design Goals

SupplyLoadComparator Output Status (OUT)
Operating Voltage RangeMAX Operating Voltage (VOVER)SUPPLY < VOVERSUPPLY ≥ VOVER
12 V to 36 V30 VVOL < 0.4 VVOH = SUPPLY

Design Description

This overvoltage protection circuit uses a high-voltage comparator with a push-pull output stage to control a P-Channel MOSFET that connects the SUPPLY to the LOAD. When the SUPPLY voltage exceeds the overvoltage threshold (VOVER), the output of the comparator goes HIGH and disconnects the LOAD from the SUPPLY by opening the P-Channel MOSFET. Likewise, when the SUPPLY voltage is below VOVER, the output of the comparator is LOW and connects the LOAD to the SUPPLY.

GUID-323154A9-44BE-42C3-BFB9-AA617FF06418-low.gif

Design Notes

  1. Select a high-voltage comparator with a push-pull output stage.
  2. Select a reference voltage that is below the lowest operating voltage range for the SUPPLY.
  3. Calculate values for the resistor divider so the critical overvoltage level occurs when the input to the comparator (+IN) reaches the comparator's reference voltage.
  4. Limit the source-gate voltage of the P-Channel MOSFET so that it remains below the device's maximum allowable value.

Design Steps

  1. Select a high-voltage comparator with a push-pull output stage that can operate at the highest possible SUPPLY voltage. In this application, the highest SUPPLY voltage is 36 V.
  2. Determine an appropriate reference level for the overvoltage detection circuit. Since the lowest operating voltage for the SUPPLY is 12 V, a 10 V zener diode (Z1) is selected for the reference (VREF).
  3. Calculate value of R3 by considering the minimum bias current to keep the Z1 regulating at 10V. A minimum bias current of 100 µA is used along with the minimum SUPPLY voltage of 12 V.
    R 3 = SUPPLY   ( min ) - V ZENER I BIAS   ( min ) = 12 V - 10 V 100 μA = 20   kΩ
  4. Calculate the resistor divider ratio needed so the input to the comparator (+IN) crosses the reference voltage (10 V) when the SUPPLY rises to the target overvoltage level (VOVER) of 30 V.
    V REF = V OVER × R 2 R 1 + R 2
    R 2 R 1 + R 2 = V REF V OVER = 10 V 30 V = 0 . 333
  5. Select values for R1 and R2 that yield the resistor divider ratio of 0.333 V by using the following equation or using the online at Voltage Divider Calculator.
    If using the following equation, choose a value for R2 in the 100 kΩ range and calculate for R1. In this example, a value of 100 k was chosen for R2.
    R 1 = R 2 V OVER V REF - 1 = 100   kΩ   30 V 10 V - 1 = 200   kΩ
  6. Note that the TLV1805 which is used in application circuit has 15 mV of hysteresis. This means that the actual switching threshold will be 7.5 mV higher than the switching threshold (VREF) when the SUPPLY is rising and 7.5 mV lower when the SUPPLY is falling. The result of the hysteresis is most easily seen in the DC Simulation curve. Since SUPPLY is resistor divided down by a factor of 3, the net impact to the SUPPLY switching threshold is 3 times this amount.
  7. Verify that the current through the resistor divider is at least 100 times higher than the input bias current of the comparator. The resistors can have high values to minimize power consumption in the circuit without adding significant error to the resistor divider.
  8. Select a zener diode (Z2) to limit the source-gate voltage (VSG) of the P-Channel MOSFET so that it remains below the device's maximum allowable value. It is common for P-Channel, power MOSFETs to have a VSG max value of 20 V, so a 16 V zener is placed from source to gate.
  9. Calculate a value for the current limiting resistor (R4). When SUPPLY rises above 16 V and Z2 begins to conduct, R4 limits the amount of current that the comparator output will sink when its output is LOW. With a nominal SUPPLY voltage of 24 V, the sink current is limited to 80 µA.
    I SINK = SUPPLY   -   V Z 2 R 4 = 24 V - 16 V 100   kΩ = 80   μA

Design Simulations

DC Simulation Results

GUID-26352338-0F99-4195-AEE0-339854D77164-low.gif

Transient Simulation Results

GUID-1167F27A-C533-47B9-989C-FE5CEABFCC44-low.gif

References:

  1. Analog Engineer's Circuit Cookbooks
  2. SPICE Simulation File SNOAA20
  3. TI Precision Labs

Design Featured Comparator

TLV1805-Q1 / TLV1805
VS 3.3 V to 40 V
VinCM Rail-to-rail
VOUT Push-Pull
VOS 500 µV
Hysteresis15 mV
IQ 135 µA
tPD(HL)250 ns
TLV1805

Design Alternate Comparator

TLV3701 / TLV370x-Q1TLC3702 / TLC3702-Q1
VS 2.5 V to 16 V4 V to 16 V
VinCM Rail-to-rail-1 V from VDD
VOUT Push-PullPush-Pull
VOS 250 µV1.2 mV
Hysteresisn/an/a
IQ 0.56 µA9.5 µA/Ch
tPD(HL)36 µs0.65 µs
TLV3701TLC3702

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale