• Menu
  • Product
  • Email
  • PDF
  • Order now
  • MCT8316ZTEVM Evaluation Module

    • SNLU291B March   2021  – August 2022 MCT8316Z

       

  • CONTENTS
  • SEARCH
  • MCT8316ZTEVM Evaluation Module
  1.   Abstract
  2.   Trademarks
  3. 1Cautions and Warnings
  4. 2Introduction
  5. 3Quick Start Guide
  6. 4Hardware and Software Overview
    1. 4.1 Hardware Connections Overview – MCT8316ZTEVM
    2. 4.2 Connection Details
    3. 4.3 MSP430FR2355 Microcontroller
    4. 4.4 LED Lights
    5. 4.5 User-Configurable Settings
    6. 4.6 Hardware Variant Settings
    7. 4.7 MCT8316Z0R Compatibility
  7. 5Hardware Setup
  8. 6Firmware and GUI Application
    1. 6.1 Downloading Code Composer Studio and Importing GUI Code
    2. 6.2 Using the eZ-FET to Program the MSP430FR2355
    3. 6.3 Importing GUI into GUI Composer
    4. 6.4 MCT8316ZTEVM GUI
  9. 7Schematics
    1. 7.1  Main Supply and Pi Filter
    2. 7.2  Connectors and Interface
    3. 7.3  USB to UART
    4. 7.4  MCU Programming and Debug
    5. 7.5  MSP430FR2355 MCU
    6. 7.6  MCT8316ZT 3-Phase Sensored Trapezoidal Integrated Driver
    7. 7.7  3.3V Buck Regulator
    8. 7.8  Status LEDs
    9. 7.9  Hardware Variant Settings
    10. 7.10 Switches and PWM Input
  10. 8Revision History
  11. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

EVM USER'S GUIDE

MCT8316ZTEVM Evaluation Module

Abstract

This document is provided with the MCT8316ZT customer evaluation module (EVM) as a supplement to the MCT8316Zx data sheet (MCT8316Z Three-Phase Sensored-Trapezoidal BLDC Motor Driver Data Sheet). This User's Guide details the hardware implementation of the EVM and how to setup and power the board.

Note:

The MCT8316ZTEVM comes automatically populated with and configured for the MCT8316Z0T. It is also compatible for the MCT8316Z0R variant (see MCT8316Z0R Compatibility), but the user will need to replace the MCT8316Z0T with the MCT8316Z0R for compatibility.

Trademarks

LaunchPad™ is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

1 Cautions and Warnings

Observe the following cautions and warnings as printed on the EVM board.

CAUTION:

GUID-7CC13EDA-5BC4-43F8-8A6D-DA5E93CED6BA-low.gif

Read the User's Guide before use.
HOT SURFACE:

GUID-205F0F0A-5CDE-4598-B85B-F2D18DA9F61B-low.gif

Caution Hot Surface! Contact may cause burns. Do not touch. Please take the proper precautions when operating.

2 Introduction

The MCT8316Z is a 4.5-V to 35-V, 8-A peak integrated three-phase gate driver IC with sensored trapezoidal control for motor drive applications. It provides three integrated half-bridges and a sensored trapezoidal algorithm capable of directly driving a 3-phase brushless-DC motor. The hardware interface variant (MCT8316ZT) integrates an adjustable buck regulator, protection features, and flexible parameter settings such as slew rate control and buck output voltage. See Table 3-1.

Table 2-1 MCT8316Z variants

Device Name

Variant

MCT8316Z0T

Buck regulator and Hardware

MCT8316Z0R

Buck regulator and SPI

The MCT8316ZTEVM includes an onboard FTDI chip to convert USB communication from the micro-USB connector into UART. An onboard MSP430FR2355 MCU translates the UART communication and onboard potentiometer into control signals and a variable duty cycle for the PWM input of the MCT8316Z. It can also provide SPI communication for the SPI variant of the MCT8316Z device. There are many user-selectable jumpers, resistors, connectors, and test points to evaluate the features of the device and configure device-specific settings.

This document serves as a startup guide to supplement the MCT8316ZTEVM. It is intended for engineers to design, implement, and validate reference hardware for the MCT8316ZT (H/W variant) along with the device data sheet.

GUID-20210126-CA0I-TWDR-QLCC-NHHFCLD5M9B5-low.pngFigure 2-1 MCT8316ZTEVM Printed Circuit Board (PCB - Top View)

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale