• Menu
  • Product
  • Email
  • PDF
  • Order now
  • DS2X0DF810 Junction Temperature Readback and Temperature Lock Range (TLR) Extension Procedures

    • SNLA386 May   2021 DS250DF810 , DS280DF810

       

  • CONTENTS
  • SEARCH
  • DS2X0DF810 Junction Temperature Readback and Temperature Lock Range (TLR) Extension Procedures
  1.   Trademarks
  2. 1Introduction
  3. 2Reading Junction Temperature Procedure
  4. 3Extending Temperature Lock Range (TLR) Procedure
  5. 4Summary
  6. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

DS2X0DF810 Junction Temperature Readback and Temperature Lock Range (TLR) Extension Procedures

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

A key parameter when using the DS2X0DF810 25-28G retimers is the temperature lock range (TLR) of the device. The TLR refers to the CDR stay-in-lock ambient temperature range that can be supported without any loss-of-lock event. In the data sheet, TLR is specified in the Electrical Characteristics in terms of both TEMPLOCK– (maximum temperature change when ramping down below the initial CDR lock acquisition ambient temperature) and TEMPLOCK+ (maximum temperature change when ramping up above the initial CDR lock acquisition ambient temperature).

The DS2X0DF810 25-28G retimers offer a method through I2C programming to extend the TLR to approximately 150°C (typical) in applications where the device junction temperature may vary beyond the default TLR range mentioned in the DS2X0DF810 data sheet. This is made possible by reading back the internal junction temperature through an on-die temperature sensor and then configuring the CDR loop filter control voltage accordingly. This method allows for the maximum change in the loop filter control voltage to tolerate all supported temperature scenarios, including worst-case scenarios when the device locks at extreme temperatures such as –40°C ambient or 110°C junction temperature.

This application note addresses the I2C programming procedure regarding how to read back the junction temperature and how to extend the device TLR based on the junction temperature readback.

2 Reading Junction Temperature Procedure

Table 2-1 provides a programming procedure to read the junction temperature from the DS2X0DF810 25-28G retimers. This procedure is beneficial for occasional debug and link monitoring.

Note: The accuracy of the on-die temperature sensor is not ensured by production testing. Through empirical observation, the temperature sensor readback exhibits a typical TJ accuracy of approximately ±7°C. Therefore, the procedure should be restricted to occasional debug use only.
Table 2-1 Programming Procedure for Reading Junction Temperature
STEP REGISTER SET OPERATION

REGISTER ADDRESS

[HEX]

REGISTER VALUE

[HEX]

WRITE MASK

[HEX]

COMMENT
Normal Retimer configuration
Perform all steps to configure the Retimer as normal. Junction temperature measurements are the most useful when the device is operating in a configuration which mimics the mission-mode configuration.
Configure Retimer for temperature readback
1 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
2 Shared Write 04 40 40 Reset Channel 0 – Channel 3 shared registers
3 Shared Write FF 20 FF Select Channel 4 – Channel 7 shared registers
4 Shared Write 04 40 40 Reset Channel 4 – Channel 7 shared registers
5 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
6 Shared Write 0F 00 FF Enable temperature detection CH0-CH3
7 Shared Write FF 20 FF Select Channel 4 – Channel 7 shared registers
8 Shared Write 0F 00 FF Enable temperature detection CH4-CH7
9 Shared Write FF 01 FF Disable broadcast write to all channels, read from channel selected in Shared Reg_0xFC
10 Shared Write FC 04 0F Select single channel
11 Channel Write 19 01 C1 Enable channel temperature detection
12 Channel Write 18 01 03 Enable channel temperature detection
13 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
14 Shared Write 0C 00 38 Configure the input to the analog-to-digital converter (ADC)
15 Shared Write 0C 02 03 Enable ADC
16 Shared Write 0C 04 04 Reset ADC
17 Shared Write 0C 00 04 Set ADC to capture Analog Voltage
18 Wait 200 µs
19 Shared Write 0C 00 02 Disable ADC to freeze value
Temperature readback
20 Shared Read 0D -- -- DSAR[7:0] = Reg_0x0E[7:0]
21 Shared Read 0E -- -- DSAR[9:8] = Reg_0x0E[1:0]
  • Decimal_representation_of_temperature_code = (Reg_0x0E and 0x03) × 256 + Reg_0x0D
  • TJ = (0.73 × Decimal_representation_of_temperature_code) – 340, in degrees C
  • Note: The numbers 256 and 340 in the previous equations are decimal numbers.
22 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
23 Shared Write 04 40 40 Reset Channel 0 – Channel 3 shared registers
24 Shared Write FF 20 FF Select Channel 4 – Channel 7 shared registers
25 Shared Write 04 40 40 Reset Channel 4 – Channel 7 shared registers
26 Shared Write FF 01 FF Enable read/write from/to channel selected in Reg_0xFC
27 Shared Write FC 04 0F Select single channel
28 Channel Write 19 00 C1 Disable channel temperature detection
29 Channel Write 18 00 03 Disable channel temperature detection

3 Extending Temperature Lock Range (TLR) Procedure

The DS2X0DF810 retimer TLR can be extended to support CDR stay-in-lock between -40°C ambient temperature to 110°C junction temperature. This is accomplished by expanding on the internal junction temperature readback procedure shown in Section 2.

To extend TLR based on the internal junction temperature readback, the complete programming procedure in Table 3-1 should be included as part of the normal retimer programming procedure. For simplicity, this procedure is written assuming all channels in the retimer are being configured at the same time. Refer to the Common Device Configurations section of the DS2X0DF810 Programming Guide for example programming procedures.

Note: Insert this procedure just prior to the step where the CDR reset is asserted and de-asserted.
Table 3-1 Programming Procedure for Each Channel to Achieve Extended TLR
STEP REGISTER SET OPERATION

REGISTER ADDRESS

[HEX]

REGISTER VALUE

[HEX]

WRITE MASK

[HEX]

COMMENT
Normal Retimer configuration
Perform all steps to configure the Retimer as normal, except for the final step, which is to assert and de-assert the CDR reset. This step will be performed at the conclusion of this Extended TLR programming procedure.
Configure Retimer for temperature readback
1 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
2 Shared Write 04 40 40 Reset Channel 0 – Channel 3 shared registers
3 Shared Write FF 20 FF Select Channel 4 – Channel 7 shared registers
4 Shared Write 04 40 40 Reset Channel 4 – Channel 7 shared registers
5 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
6 Shared Write 0F 00 FF Enable temperature detection CH0-CH3
7 Shared Write FF 20 FF Select Channel 4 – Channel 7 shared registers
8 Shared Write 0F 00 FF Enable temperature detection CH4-CH7
9 Shared Write FF 03 FF Enable broadcast write to all channels, read from channel selected in Shared Reg_0xFC
10 Shared Write FC 04 0F Select single channel
11 Channel Write 0A 00 0C Release CDR from reset
12 Channel Write 14 80 80 Force-enable signal detect to ensure all channels are powered on prior to reading device temperature
13 Channel Write 19 01 C1 Enable channel temperature detection
14 Channel Write 18 01 03 Enable channel temperature detection
15 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
16 Shared Write 0C 00 38 Configure the input to the analog-to-digital converter (ADC)
17 Shared Write 0C 02 03 Enable ADC
18 Shared Write 0C 04 04 Reset ADC
19 Shared Write 0C 00 04 Set ADC to capture Analog Voltage
20 Wait 200 µs
21 Shared Write 0C 00 02 Disable ADC to freeze value
Temperature readback and Loop Filter Voltage calculation
22 Shared Read 0D -- -- DSAR[7:0] = Reg_0x0E[7:0]
23 Shared Read 0E -- -- DSAR[9:8] = Reg_0x0E[1:0]
  • Decimal_representation_of_temperature_code = (Reg_0x0E and 0x03) × 256 + Reg_0x0D
  • LPF_Setting = 0.44 × Decimal_representation_of_temperature_code – 55
    • If (LPF_Setting < 120), then LPF_Setting = 120
    • If (LPF_Setting > 210), then LPF_Setting = 210

  • Note: The numbers 256, 55, 120, and 210 in the previous equations are decimal numbers.
Configure Loop Filter Voltage
24 Shared Write FF 03 03 Enable broadcast write to all channels, read from channel selected in Shared Reg_0xFC
25 Channel Write 9D LPF_ Setting FF Configures the Loop Filter Voltage based on the results of the previous equation
26 Channel Write 17 25 FF Enable extended temperature lock range
De-activate device temperature sensing
27 Shared Write FF 10 FF Select Channel 0 – Channel 3 shared registers
28 Shared Write 04 40 40 Reset Channel 0 – Channel 3 shared registers
29 Shared Write FF 20 FF Select Channel 4 – Channel 7 shared registers
30 Shared Write 04 40 40 Reset Channel 4 – Channel 7 shared registers
31 Shared Write FF 03 FF Enable writing to all channels
32 Channel Write 19 00 C1 Disable channel temperature detection
33 Channel Write 18 00 03 Disable channel temperature detection
34 Channel Write 14 00 80 Undo force-enable of signal detect
Conclude normal Retimer configuration
35 Channel Write 0A 0C 0C Assert CDR reset
36 Channel Write 0A 00 0C De-assert CDR reset
37 Shared Write FF 01 01 Disable Broadcast write operation

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale