SNLA308A April 2019 – October 2020 DS90UB941AS-Q1 , DS90UH941AS-Q1
All trademarks are the property of their respective owners.
The DS90Ux941AS-Q1 splitter and cropping functions allow system designers to use cost-effective IVI systems with only a single AP for delivering content to two symmetric or asymmetric displays. An application processor can receive and combine two video frames into a superframe, and perform the necessary video data formatting to ensure that the data is compatible with the DS90Ux941AS-Q1 signal processing functions (see Figure 1-1). The DS90Ux941AS-Q1 performs further video formatting and splits of the superframe into two symmetric frames before forwarding them to the compatible FPD-Link III deserializers and attached displays. If necessary, the DS90Ux941AS-Q1 can also crop either one or both resultant frames for the formation of asymmetric frames before forwarding the frames to the deserializers and asymmetric displays.
The DS90Ux941AS-Q1 supports superframe options with the following formats:
For the first two options, the DS90Ux941AS-Q1 reorganizes the superframe into an alternating pixel format for easy splitting at the DS90Ux941AS-Q1 output. For the Alternate Pixel option, the superframe is already in the proper format for splitting.
For proper transition between operating modes, only enable 3D modes when the DSI input is disabled.