• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TPS7H500x-SP Evaluation Module User's Guide

    • SLVUCD0 February   2022 TPS7H5002-SP , TPS7H5003-SP , TPS7H5004-SP

       

  • CONTENTS
  • SEARCH
  • TPS7H500x-SP Evaluation Module User's Guide
  1.   Trademarks
  2. 1Introduction
    1. 1.1 Features
    2. 1.2 Applications
  3. 2EVM Setup and Quick Start Guide
  4. 3EVM Connectors and Test Points
  5. 4PCB Layouts
  6. 5Schematics
  7. 6Bill of Materials
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

TPS7H500x-SP Evaluation Module User's Guide

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

This board enables the TPS7H5001/2/3/4EVM-CVAL to be connected to other components needed to quickly prototype and evaluate a complete power converter design. The TPS7H5001EVM-CVAL is placed on an open test board similar to the board used in the TPS7H5001-SP Lookahead Total Ionizing Dose (TID) radiation report. Adding test points and voltage terminals is the only major change to the design that was needed to facilitate probing the TPS7H5001/2/3/4EVM-CVAL without additional hardware. Minor changes were made to the BOM for manufacturability purposes.

1.1 Features

This EVM has the following features:

  • Synchronous rectification outputs with adjustable dead time
  • 0.613-V ±1% Voltage reference overtemperature, radiation, and line and load
  • Adjustable slope compensation and soft start
  • Configurable duty cycle limit

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale