• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TPS92630EVM ESD Test Report

    • SLVAFF2 July   2022 TPS92630-Q1

       

  • CONTENTS
  • SEARCH
  • TPS92630EVM ESD Test Report
  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Test Conditions
    2. 1.2 Test Setup Diagrams
  4. 2Test Results
  5. 3Conclusion
  6. 4References
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

TPS92630EVM ESD Test Report

Abstract

This application note presents ESD contact discharge test results for the TPS92630EVM, 3-channel LED driver, and demonstrates how ISO 10605 standards can be met for this device.

Automotive industry in-vehicle use cases:

  • Illuminate driver for driver monitoring systems (DMS)
  • Power supply for indicator LED in side mirror in blind spot detection applications

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

A fully-compliant ESD chamber and equipment is used for this testing to conduct the following testing conditions.

The TPS92639EVM was protected with the ESD2CAN24-Q1, an automotive dual-ESD protection diode, soldered on the LED driver signal output and the LED loads of the evaluation module.

1.1 Test Conditions

The following:

  • Disconnected from power supply
  • Contact discharge:
    • ±8 kV, 150 pF at 0.33 kΩ
    • ±15 kV, 330 pF at 2 kΩ
    • ±25 kV, 330 pF at 2 kΩ
  • Three discharges with a 3-second interval
  • Loaded and open configuration

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale