• Menu
  • Product
  • Email
  • PDF
  • Order now
  • PoE Powered Devices Debug Guidelines

    • SLVAF74 July   2021 TPS2372 , TPS2373 , TPS23730 , TPS23731 , TPS23734 , TPS2375 , TPS2375-1 , TPS23750 , TPS23751 , TPS23752 , TPS23753A , TPS23754 , TPS23754-1 , TPS23755 , TPS23756 , TPS23757 , TPS23758 , TPS2376 , TPS2376-H , TPS2377 , TPS2377-1 , TPS23770 , TPS2378 , TPS2379

       

  • CONTENTS
  • SEARCH
  • PoE Powered Devices Debug Guidelines
  1.   Trademarks
  2. 1Introduction
  3. 2Preparation and Measurement Techniques
    1. 2.1 Important PoE Signals
    2. 2.2 Lab Equipment
    3. 2.3 Measurement Techniques
    4. 2.4 Board Preparation
  4. 3Narrowing Down the Problem Area
    1. 3.1 Schematic Areas
    2. 3.2 Narrowing Down the Area On Board
  5. 4Common Issues
  6. 5Conclusion
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

PoE Powered Devices Debug Guidelines

Trademarks

Sifos is a registered trademark of Sifos Technologies, Inc..

All trademarks are the property of their respective owners.

1 Introduction

This guide has three main parts. The first part is the preparation work before debugging. Sometimes the preparation work can take an hour or more, but good preparation decreases overall debugging time. The second part of the guide covers the first part of the debug process: narrowing down what is causing the issue. PoE plus DC/DC designs can be broken up into sections, and this application report guides you through how to check if one or more of these sections are suspect in the problem. The third part of this guide covers common issues and common resolutions. For example, if the design has the parallel MOSFET in an active clamp forward that breaks during shutdown, what are the issues that usually cause that? This list is not exhaustive because there are many components in PoE designs and they can break in different ways and for different reasons. However, this guide should aid in the first steps of the debug process for most PoE designs.

Note: This document only covers flybacks and active clamp forward topologies. These are the main two topologies used in PoE applications because they provide good comprises of size, cost, and performance for a nominal PoE input voltage range (37 V–57 V) to a typical output voltage range (3.3 V–24 V) while providing isolation.

2 Preparation and Measurement Techniques

Part of the current TI strategy is to provide working reference designs that can be copied. The first recommendation is to find the closest reference design possible to the design being worked on. Look for the same IC, the same topology (for example, synchronous flyback), and the same output voltage and power level. If there is not a close design, contact the PoE applications engineer through E2E for an internal search. Next, evaluate any parts that are different, whether it be a transformer, a MOSFET, a resistor size, and so forth. Question why the part is different. List all the reasons how these parts are different (for example, different gate capacitance, different reverse recovery time, different voltage rating, different package size). These may be the first clues to why the design is experiencing problems, but the TI reference design is not. Review the PoE PD Schematic Review Guidelines application report for component variations.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale