• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Shunt Regulator Design Procedures for Secondary Feedback Loop in Isolated Converter

    • SLVAF37 January   2021 ATL431LI

       

  • CONTENTS
  • SEARCH
  • Shunt Regulator Design Procedures for Secondary Feedback Loop in Isolated Converter
  1.   Trademarks
  2. 1Introduction
    1. 1.1 TL431 as a Type-2 Amplifier
    2. 1.2 TL431 Solution with Isolation
  3. 2Design Procedures
    1. 2.1 Design Considerations for Optocoupler
    2. 2.2 Design Considerations for Biasing Circuit
    3. 2.3 Schematic Analysis and Waveforms
  4. 3Summary
  5. 4References
  6. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Shunt Regulator Design Procedures for Secondary Feedback Loop in Isolated Converter

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

1.1 TL431 as a Type-2 Amplifier

Figure 1-1 is a general current-mode control converter. This type of non-isolated converters integrate the EA (error amplifier) and Vref as parts of feedback control loop. And Type-2 amplifier network provides optimal compensation in the loop.

GUID-20210119-CA0I-CTHV-J69Q-9GZHDRF0HLGL-low.png Figure 1-1 Feedback Loop in Non-Isolated Current-Mode Control Converter

On the basis of the composition of TL431, Figure 1-2 shows how it can be used as a standard EA.

GUID-20210119-CA0I-DSVK-0WR7-FW9VGT7J3JB3-low.png Figure 1-2 TL431 Used As A Type-2 Amplifier

The pullup resistor (Rbias) value should be chosen to meet the minimum cathode current requirement, this is to provide sufficient bias current to TL431 under all circuit conditions.

1.2 TL431 Solution with Isolation

TL431 has been used widely in isolated power supply applications and it provided design benefits of reducing the cost of feedback loop, taking up little board space within the performance tradeoff from the standard error amplifier and a precision reference.

GUID-20210119-CA0I-HW27-LBQF-DZLZNBRKCCFF-low.png Figure 1-3 Flyback with Optocoupler Isolation with TL431

Further detail from Figure 1-3, we now understand TL431 is powered from output of converter. And the amount of current flowing through the Rbias and the optocoupler diode to the cathode of TL431 are driving the gain and operation of the circuit. Figure 1-4 shows typical TL431 in conjunction with optocoupler for isolated feedback control.

GUID-20210119-CA0I-GPCH-RLQ1-CWKHFTRPC8TG-low.png Figure 1-4 TL431 In Conjunction with Optocoupler for Isolated Feedback

As described, the bias current at both primary and secondary side are controlling the gain and frequency response of the circuit. However, it is very complicated analysis and even latest controllers have built the primary side bias, including current source and resistors, inside. Hence, we have options to follow design procedures for bias circuit of secondary side feedback.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale