• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Detecting Short to Battery and Ground Conditions with TI Motor Gate Drivers

    • SLVAEV8 June   2020 DRV8106-Q1 , DRV8701 , DRV8702-Q1 , DRV8702D-Q1 , DRV8703-Q1 , DRV8703D-Q1 , DRV8705-Q1 , DRV8706-Q1

       

  • CONTENTS
  • SEARCH
  • Detecting Short to Battery and Ground Conditions with TI Motor Gate Drivers
  1.   Detecting Short to Battery and Ground Conditions with TI Motor Gate Drivers
    1.     Trademarks
    2. 1 How VDS Monitors Detect OCP Conditions
    3. 2 Using VDS Monitors to Identify Fault Types
    4. 3 Conclusion
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Detecting Short to Battery and Ground Conditions with TI Motor Gate Drivers

Detecting Short to Battery and Ground Conditions with TI Motor Gate Drivers

Overcurrent protection (OCP) is a key protection feature in preventing damage to motor systems. It is important for motor drivers to monitor the FETs closely and shut them down in a safe manner in the case of an overcurrent or fault condition. VDS monitors are used in gate drivers to detect overcurrent conditions and provide fault protection. This article covers how VDS monitors detect OCP conditions and explains how gate drivers with an SPI interface can use the location of an OCP condition to identify where the fault occurred in the system.

Trademarks

All other trademarks are the property of their respective owners.

1 How VDS Monitors Detect OCP Conditions

VDS monitors are connected at the drain and source of the FET. The voltage across the drain and source provides information on how much current is running through each FET. As shown in Figure 1, each FET has its own VDS monitor.

VDS-Monitor-Schematic.gifFigure 1. VDS Monitor Schematic

With TI motor gate drivers, designers can set VDS overcurrent protection threshold values based on the expected current through the FETs and failure conditions they are trying to protect against. This can be done many ways depending on the device used. For example, on DRV8705-Q1 it can be adjusted through VDS_LVL register settings for the SPI interface. For hardware interfaces, designers can set the desired threshold values by connecting resistors to the appropriate pin. Specifications for resistor values and threshold values vary from one device to another and can be found in each device’s datasheet.

In SPI devices, designers also have the option to set the OCP deglitch time. The duration of the overcurrent condition must be greater than the OCP deglitch time for an OCP condition to occur through the VDS register. OCP deglitch time preferences can vary depending on the time it takes to charge the FETs. The longer it takes to charge the FETs, the longer the OCP deglitch time is to ensure the FETs turn on and prevent false OCP conditions. For devices with a hardware interface, the OCP deglitch time falls within a range, specific to each device, which cannot be changed. In the event of an OCP condition, the FETs are disabled to prevent any damage. The specifics of a device’s response and recovery from an OCP condition vary from one to device to another.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale