• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Designing Boost Converter TPS61022 for Supercap Backup Power Applications

    • SLVAER4 August   2020  – MONTH  TPS61022

       

  • CONTENTS
  • SEARCH
  • Designing Boost Converter TPS61022 for Supercap Backup Power Applications
  1.   Trademarks
  2. 1Introduction
  3. 2Proposed Circuit Principle
  4. 3Loop Stability, Feedforward Capacitor Selection
  5. 4Schematic and Bench Test Results
    1. 4.1 Schematic
    2. 4.2 Bench Test Results
  6. 5Summary
  7. 6References
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Designing Boost Converter TPS61022 for Supercap Backup Power Applications

Trademarks

All other trademarks are the property of their respective owners.

1 Introduction

Smart meters must continue to operate during brief power outages and send notification messages through a wireless radio, which consumes significant amount energy. As the output voltage of one cell supercap is not higher than 2.7 V, a boost converter is needed to step up the output voltage to power the GSM/GPRS module or MCU. The GSM/GPRS module voltage is normally higher than 3.6 V. The low input voltage boost converter can fully utilize the energy of the supercap and extend the backup power time.

The TPS61022 provides a power-supply solution for portable equipment and IoT devices powered by various batteries and super capacitors. The TPS61022 has minimum 6.5-A valley switch current limit over the full temperature range. With a wide input voltage range of 0.5 V to 5.5 V, the TPS61022 supports supercapacitor backup power applications, which may deeply discharge the supercapacitor.

Figure 1-1 is the schematic in the TPS61022EVM user’s guide designed for a 3.0 V to 4.2 V lithium-ion battery input, 5-V output power supply application. However, for low VIN of 0.5 V to 2.7 V supercap backup power application, an extra feedforward capacitor and big output capacitance is needed to increase the phase margin to make the loop stable.

GUID-5F44C732-EF2E-483E-A8CC-E122F8032101-low.gifFigure 1-1 TPS61022 EVM Schematic

This application report introduces how to select the TPS61022 external components for supercap backup power applications. Detailed calculation methods and bench test results are presented to verify the proposed circuit.

2 Proposed Circuit Principle

Figure 2-1 shows the theoretical circuit of the TPS61022 boost converter circuit in a supercap backup power system. The Vsys is the brief power, coming from other DC/DC converter or the grid. The TPS61022 has a MODE pin to set the operation mode. When the mode is logic high, the device operates at forced pulse width modulation (PWM) mode. At forced PWM mode, the device keeps switching with 1 MHz (VIN > 1.5 V) and 600 kHz (VIN < 1.0 V) disregarding the loading. This results in very low efficiency at light load conditions. There may be a reverse current from VOUT to charge the supercap by setting the MODE pin to logic high if the voltage of Vsys is higher than the TPS61022 setting output voltage. When the MODE is connected to a logic low voltage, the device works in auto PFM mode and there is no reverse current from VOUT to VIN by using the following configurations:

  • It is recommended to connect the MODE pin to GND to set the device working at auto PFM mode. Efficiency at light load is increased and total supercap discharging time is extended.
  • Set the TPS61022 VOUT 3 to 5% less than Vsys. The device does not switch when Vsys exists.
  • The EN pin is connected to VIN to make the device stay in theenable state. The TPS61022 device consumes very little quiescent current (3.0 µA into VIN pin and 32 µA into the VOUT pin).

When the brief power Vsys browns out and drops less than the TPS61022 programmed output voltage VOUT, the TPS61022 starts switching and maintains VOUT at the programmed output voltage level.

GUID-20200728-CA0I-GWLM-RGRB-7MGSQXKZGKPH-low.gifFigure 2-1 TPS61022 Boost Converter in Supercap Backup Power Applications

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale