• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Loop Response Considerations in Peak Current Mode Buck Converter Design

    • SLVAE09B July   2018  – August 2021 TPS560430

       

  • CONTENTS
  • SEARCH
  • Loop Response Considerations in Peak Current Mode Buck Converter Design
  1.   Trademarks
  2. 1Introduction
  3. 2Peak Current Mode Loop Modeling
    1. 2.1 Overall Control Block Diagram and Transfer Function Derivation
    2. 2.2 Inside Current Loop Model
    3. 2.3 Overall Loop Model
    4. 2.4 Inductor and Output Capacitor Design Limits
    5. 2.5 The Equation to Calculate Bandwidth and Phase Margin
  4. 3Inductor and Output Capacitor Design
    1. 3.1 Inductor Design
    2. 3.2 Output Capacitor Design
    3. 3.3 Simulation and Bench Verification
  5. 4Summary
  6. 5References
  7. 6Revision History
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Loop Response Considerations in Peak Current Mode Buck Converter Design

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The TPS560430 regulator is an easy-to-use synchronous step-down DC/DC converter operating from 4-V to 36-V supply voltage. It is capable of delivering up to 600-mA DC load current in a very small solution size. The family has different versions applicable for different applications, 1.1-MHz and 2.1-MHz switching frequency, PFM and FPWM, adjustable and fixed output voltage. The device is suitable for a wide range of applications from industrial to automotive for power conditioning from an unregulated source. The TPS560430 employs peak-current mode control with internal loop compensation, which reduces design time, and requires few external components.

A lot of PCM loop models are available for system design. The most popular model is provided in [2]. The model predicted the sample and hold effects in the current loop, while using a three-terminal switch model to calculate power stage small signal model. Using this method, a simplified loop model is provided in [3], and an equivalent circuit is obtained to simulate the loop response. However, if all of the models require simulation tools to draw the bode plot, then find a crossover frequency and phase margin based on the bode plot. Besides, the transfer function of inner current loop is quite complex, making it hard to understand how it impacts the whole loop response. In this document, a simple equation is provided to calculate bandwidth. The phase margin is obtained by simplifying the inside current loop as a single pole. The inner current loop stability criteria can be obtained based on the model. Each zero and pole in the model has a clear physical meaning, making it easy to analyze the impact of each component value on the loop response. The inductor and output capacitor design procedure of the internally compensated PCM buck converter is given using the model. The model accuracy is verified by both simulation and bench measurement results.

2 Peak Current Mode Loop Modeling

2.1 Overall Control Block Diagram and Transfer Function Derivation

Figure 2-1 shows the simplified schematic for the PCM buck converter.

GUID-774F8D55-494B-4540-8CE5-E88EDB77D866-low.gifFigure 2-1 Simplified Schematic for PCM Buck Converter
GUID-7CE0E554-1C30-4A7E-984F-400664070D4F-low.gifFigure 2-2 Overall Control Implementation

Figure 2-2 shows the overall control block model where:

  • Gdi(s) is the duty cycle to iL transfer function.
  • ZO(s) is the transfer function of output impedance.
  • Gdiv(s) is the gain of the feedback resistor network.
  • GEA(s) is the transfer function of the error amplifier with certain compensation.
  • Fm is the gain of PCM PWM comparator.
  • Ri is the current sensing resistor.
  • He(s) is the transfer function model of inductor current sampling-hold effect.

Equation 1 shows the transfer function from the inductor current to the output voltage.

Equation 1. GUID-55305D7F-267C-4847-AC11-B3C5F273AEFE-low.gif

Gdi(s) is the duty cycle to iL transfer function.

Equation 2. GUID-7F275364-CA09-4806-A4E1-523E5C5C5241-low.gif

The internal loop compensation is designed so that the crossover frequency is much higher than the corner frequency, 1/(2π√LCO). For crossover frequency and higher frequency, Equation 2 can be simplified as Equation 3.

Equation 3. GUID-327DD9FA-D133-401F-AA31-8ECEF76C6789-low.gif

The sensed inductor current, external ramp, and the output of error amplifier VCOMP are compared, which determines when to turn off the high side MOSFET, hence the duty cycle is determined. Fm is the comparator gain. fSW is the switching frequency. Sn is the on-time slope of the sensed-current waveform and Se is the external ramp slope.

Equation 4. GUID-6652F466-29DC-4E6D-97CD-752F7EB408C0-low.gif

where

  • GUID-EA853B6B-7275-4E2B-8B25-2E41BC4D43BD-low.gif
    GUID-1EC2AE3E-F7AB-4739-BF2C-06DA442B0D67-low.gif

He(s) is the transfer function model of inductor current sampling-hold effect. [2]2:

Equation 5. GUID-7C178B59-54A2-42CE-AF18-A2F5079831C1-low.gif

Equation 6 shows the transfer function of the feedback.

Equation 6. GUID-0023F73F-49AB-493F-B345-433A09BE70A7-low.gif

Equation 7 shows the transfer function of the error amplifier with certain compensation.

Equation 7. GUID-F539C154-B477-4E6A-A8F4-CF43450DDF2E-low.gif

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale