• Menu
  • Product
  • Email
  • PDF
  • Order now
  • How Single Pulse Mode in Boost Converter Saves the Output Capacitor

    • SLVA997A November   2018  – July 2021 TPS61322

       

  • CONTENTS
  • SEARCH
  • How Single Pulse Mode in Boost Converter Saves the Output Capacitor
  1.   Trademarks
  2. 1Traditional Power-Save Mode Control Scheme
  3. 2Single Pulse Power Save Mode Control Scheme
  4. 3Output Ripple Calculation
  5. 4Bench Result
  6. 5Conclusion
  7. 6Revision History
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

How Single Pulse Mode in Boost Converter Saves the Output Capacitor

Trademarks

All trademarks are the property of their respective owners.

1 Traditional Power-Save Mode Control Scheme

The traditional power-save mode use a low power voltage comparator to enable and disable the control loop under light load. When the output voltage reaches the target value, all the internal blocks will be disabled except the voltage comparator and reference voltage. It is fundamentally a burst-mode-control topology. In systems whose output load is at the boundary of power save mode and normal PWM mode, the device can turn on and off the control loop a number of times. To minimize the probability of the device switch between these two modes, a high hysteresis is added. Then DC output voltage is higher than the nominal value in such kind of control schemes. Typically, the DC voltage in power save mode is 0.5% to 3% higher than the nominal value. Take the TPS61021A as the example, Figure 1-1 is the typical operation behaviors of TPS61021A at light load.

GUID-A61AFDE7-A209-4912-A3C6-69C4A671BE4C-low.gif Figure 1-1 Traditional Power Save Mode Control Scheme

When the output load decreases, the error amplifier output is clamped at a certain level. Then the output voltage increases and the devices enters power save mode. During the switching period, the control loop is active and continue to output switching signals until the output voltage hits the PFM reference voltage (0.8% percent higher than the nominal voltage). Then the control loop commands the device stopping switching but actually the device will continue to switch for some cycles because of the internal comparator delay. After that, the device stops switching finally. During the non-switching period, the load is supplied by the output capacitor and the output voltage declines. When the FB voltage drops below the PFM reference voltage, the device starts switching again to ramp up the output voltage after some delay time of the comparator,.

This control scheme is very simple and effective, but it introduces high output ripple because of the multiple switching pulses in one power save mode cycle.

2 Single Pulse Power Save Mode Control Scheme

The TPS61322xx is a low quiescent, high efficiency synchronous boost converter family based on hysteretic current control topology. The TPS61322xx is designed for systems which need a constant on and quiet power rail. The input source can be one cell alkaline battery, CR2032, and lithium battery. Figure 2-1 shows the typical application schematic of TPS61322xx.

GUID-2824771E-F1CD-48A4-B98D-7558CF75AFAA-low.gifFigure 2-1 Single Pulse Control Scheme

The TPS61322xx uses single pulse power save mode and keeps the output voltage the same over all the load range. The typical control scheme is shown in Figure 2-2

GUID-B681E366-EC6D-4ACA-A4E1-743D9F347AA3-low.gifFigure 2-2 Single Pulse Control Scheme

There are 3 operation subintervals for TPS61322xx at light load: on-phase, off-phase and stop-phase. During on-phase, the low-side MOSFET is ON and high-side MOFET is OFF, the input source charges the inductor and the subsystem is powered by the output capacitor. The inductor current ramps up until triggers the hysteresis current Ihys, then the on-phase ends and the off-phases starts. During off-phase, the low-side MOSFET is OFF and high-side MOSFET is ON. The inductor charges the output capacitor and powers the sub-system at the same time. The inductor current ramps down until trigger zero current, then the stop-phase starts. During stop-phase, both low-side and high-side MOSFET are OFF and all the energy is from the output capacitor. The internal control loop is always active and regulate the stop-phase time.

This control scheme helps reduce the output capacitor significantly because only one current pulse is output in each power save mode cycle.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale