Microsoft and Excel are registered trademarks of Microsoft Corporation.
MATLAB is a registered trademark of The MathWorks, Inc..
All trademarks are the property of their respective owners.
Peak current mode control is widely used in buck controllers and converters due to its advantages for good dynamic performance and easy compensation. Most peak current mode converters have a COMP pin and customers can implement type 2 or type 3 external compensation by adjusting external resistors and capacitors. In recent years, internal compensation attracts more and more attention to reduce solution size and achieve simple application design. The TPS62933 is a buck converter with an internally compensated peak current mode that supports 3.8- to 30-V input voltage and maximum 3-A output current. The device has superior features like low IQ and a wide output voltage range. Compared to the conventional PCM devices, it does not need external resistors or capacitors for compensation setting, but the stability restriction limits the range of inductance and output capacitance.
For common applications, components can be selected based on the recommended table and implement fast design for application. For special application design to choose large output capacitance or small output capacitance, a stability design method is proposed in this application report. The application with a feedforward capacitor is not included in the analysis.
Figure 2-1 shows the schematic of a PCM buck converter. A type 2 compensation is used to ensure the stability of the converter.
The loop response model of PCM buck converters is introduced in the application report(2). Figure 2-2 shows the bode plot.
In the loop response of PCM converters, the DC gain is affected by output current.
In TPS62933, the DC gain, fP1_EA, fP2_EA, and fZ_EA are all determined by the device internal compensation circuit, which is expressed as Equation 1 and Equation 2.
where
For the application with all MLCC or small ESR output capacitors, fZ_OUT is at high-frequency range and has limited effects on converter stability.
where
fP_ci is a pole introduced by the inside current loop and related with device slope compensation. Its expression for TPS62933 is shown as Equation 5.
For system loop stability, a –20 dB/dec slope near crossover frequency is ideal for loop gain, since that can normally bring sufficient phase margin(3).
Figure 2-2 shows the loop gain slope of the PCM converter changes from 0 to –20 dB/dec at the initial pole frequency, fP1_EA. At pole fP_OUT, the loop gain slope changes to –40 dB/dec. With the compensation of zero fZ_EA, the gain slope becomes –20 dB/dec and the gain curve crosses 0 dB with this slope. That could bring sufficient phase margin for the converter.
Figure 3-1(a) illustrates that the converter crossover frequency fc becomes lower with reduced pole frequency fP_OUT. If fc < fZ_EA, the zero fZ_EA is out of crossover frequency and loop gain crosses 0 dB with a –40 dB/dec slope. If these conditions occur, they may cause insufficient phase margin.
Equation 4 shows that pole fP_OUT is inversely related with output capacitance CO. Reducing CO can make both fP_OUT and fc increase. As shown in Figure 3-1(b), after increasing the pole frequency fP_OUT, fZ_EA could be smaller than the crossover frequency fc and the loop gain crosses 0 dB with a –20 dB/dec slope. These conditions could normally ensure converter phase margin.
Based on the previous analysis, use Equation 6 to calculate the limitation for –20 dB/dec slope at gain crossover frequency:
As Equation 2 shows, fZ_EA is fixed at 10.6 kHz for TPS62933. To get the relation between output capacitance Co and fc, first calculate the relation between gain and frequency using Equation 7 and Equation 8.
where
Equation 7 and Equation 8 can be simplified as:
With Equation 4, Equation 6, and Equation 10, the upper limit for output capacitance is calculated using Equation 11.
Substituting parameters in Equation 1 and Equation 2, the upper limit for TPS62933 is:
Normally for a buck converter, a 45 degree phase margin can be achieved with –20 dB/dec slope at gain crossover frequency. But for a buck regulator with peak current-mode control, when a larger inductance is used, the frequency of the inner current loop pole fP_ci will be lower and bring more phase drop at the gain crossover frequency. These conditions may cause a phase margin lower than 45 degrees, even with –20 dB/dec crossing. Therefore, the capacitance upper limit for a 45 degree phase margin is also deducted in this section.
Figure 3-2 is a bode plot of a PCM buck converter with –20 dB/dec crossing. fZ_OUT and fP2_EA are normally at very high frequency so their effects on phase margin at gain crossover frequency can be ignored at first. Pole fP1_EA is at a very low frequency and brings about –90° phase drop at gain crossover frequency.
Next, calculate the phase margin using Equation 13. Equation 14 constitutes the limitation to make the phase margin larger than 45 degrees.
Calculate gain crossover frequency fcross using Equation 15, Equation 16 and Equation 17, based on Figure 3-2.
Derive fcross using equation Equation 18:
Substituting Equation 1, Equation 2, and Equation 4 into Equation 18, fcross is expressed with:
Substituting Equation 2, Equation 4, Equation 5, and Equation 19 into Equation 14 and ignoring ESR impacts, the upper limit for output capacitance for phase margin restriction is calculated using the following example equation:
(50*(111936*IOUT - 4460544))/(441013* IOUT *VOUT*(422400/ IOUT + (8954880000/ IOUT + 178421760000/ IOUT ^2 + (2500* VIN ^2* fsw ^2)/(24649*(4356000*L + VIN - 2* VOUT)^2) - (3180000* VIN *fsw)/(157*(4356000*L + VIN - 2* VOUT)) + (84480000* VIN * fsw)/(157* IOUT *(4356000*L + VIN - 2* VOUT)) - (267632640000* VIN * fsw)/(8321* IOUT ^2*(4356000*L + VIN - 2* VOUT)) + (10560000* VIN ^2* fsw ^2)/(1306397* IOUT *(4356000*L + VIN - 2* VOUT)^2) + (11151360000* VIN ^2* fsw ^2)/(69239041* IOUT ^2*(4356000*L + VIN - 2* VOUT)^2) + 112360000)^(1/2) - (50* VIN * fsw)/(157*(4356000*L + VIN - 2* VOUT)) - (105600* VIN * fsw)/(8321* IOUT *(4356000*L + VIN - 2* VOUT)) + 10600))
Since the expression for output capacitance upper limit with phase margin restriction is very complicated, an example of how to use Microsoft® Excel® or MATLAB® for the calculation is introduced in Section A.