• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Improving Efficiency at Higher Loads with High Switching Frequencies

    • SLUAAA5 June   2021 TPS54218 , TPS628501-Q1 , TPS628502-Q1 , TPS628510 , TPS628511 , TPS628512

       

  • CONTENTS
  • SEARCH
  • Improving Efficiency at Higher Loads with High Switching Frequencies
  1.   Trademarks
  2. 1Introduction
  3. 2Main Sources of Power Losses in Synchronous Buck Converters
  4. 3Design Example
  5. 4Summary
  6. 5References
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Improving Efficiency at Higher Loads with High Switching Frequencies

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

With the never-ending trend of faster data rates, smaller form factors, and increased power density, board space is becoming gradually scarcer. This makes the job of the power-supply designer increasingly difficult as trying to fulfill all the design requirements, while keeping solution size to a minimum, is no small feat.

One way to go about minimizing the footprint that the power supply leaves on the total design is to choose a converter with a high switching frequency. With higher switching frequencies, design requirements such as output current ripple, output voltage ripple, and load transient can be achieved by using less inductance and output capacitance. This reduces solution size and decreases the total BOM cost of the power supply.

One of the disadvantages of going for higher switching frequencies is increased switching losses. The increased switching losses do not always correlate to decreased efficiency throughout the output current range. It should not be overlooked that switching losses are only one part of the total losses that occur during the operation of a buck converter. As a matter of fact, at higher currents, the conduction losses become the dominant contributor of power loss.

TI’s TPS628512 is a high frequency synchronous buck converter with a small 1.6-mm x 2.1-mm package which provides a small solution size optimized for space constrained applications. Later on in this application note, the TPS628512 will be compared with the TPS54218 to show the impact of conduction losses, in particular, conduction losses in the inductor, on the final efficiency.

2 Main Sources of Power Losses in Synchronous Buck Converters

There are three main sources of power loss in synchronous buck converters: quiescent losses (static losses), switching losses and conduction losses. In today’s buck converters the quiescent losses generally represent only a small percentage of the total losses when the load at the output of the converter is above a few tens of milliamps. This application note looks at relatively higher currents, in which case, the switching and conduction losses play a much bigger factor than the quiescent losses – which can be neglected.

The following two sections will briefly go through the causes of switching losses and conduction losses in synchronous buck converters.

Switching Losses

Switching losses in synchronous buck converters are the result of charging and discharging the gate to drain and gate to source capacitances of the power MOSFETs when they are turned on and off. These losses can be calculated with the following equations:

Equation 1.
Equation 2.

Where:

  • PSW-TURN ON and PSW-TURN OFF are the switching losses caused by turning-on and turning-off the MOSFET respectively
  • VIN is the input voltage
  • IOUT is the output current
  • fSW is the switching frequency
  • ΔTON is the turn-on time of the MOSFET
  • ΔTOFF is the turn-off time of the MOSFET
Important to note is that the switching losses are linearly proportional with the switching frequency and with the output current.

Figure 2-1 MOSFET Turn-on and Turn-off

Conduction Losses

One part of the conduction losses (Joule losses) in a buck converter are due to the drain-source on-state resistance of the power MOSFETs:

Equation 3.
Equation 4.

and the other part is due to the DCR of the inductor:

Equation 5.

Where:

  • PON-HIGH and PON-LOW are the conduction losses in the high-side and low-side MOSFETs respectively
  • PDCR are the conduction losses due to the resistance of the inductor
  • RDS(ON)-HIGH and RDS(ON)-LOW are the drain-source on-state resistances of the high-side and low-side MOSFETs respectively
  • IHIGH-RMS and ILOW-RMS are the RMS values of the current flowing through the high-side and low-side MOSFETs respectively
  • VOUT is the ouptut voltage
  • IP is the peak of the inductor current
  • IV is the valley of the inductor current

What is important to notice from these equations is that the conduction losses are dependent on the square of the RMS value of the current flowing through the particular MOSFET and through the inductor. And unlike the switching losses they are independent of switching frequency, as long as the inductor current ripple is held constant.

Figure 2-2 shows a calculated example efficiency curve of a synchronous buck converter plotted on the left y-axis along with the corresponding switching and conduction losses plotted on the right y-axis with respect to output current. This figure clearly displays how, due to the dependency on the square of the output current, at a certain point the conduction losses become the dominating factor and at higher currents their effect on efficiency is much more significant than that of the switching losses. In general, the switching losses and conduction losses are equal near the peak of the efficiency curve.

Figure 2-2 How Conduction and Switching Losses Vary with Output Current

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale