• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Thermal Foldback Feature on SmartAmps

    • SLAA937 June   2020 TAS2110 , TAS2562 , TAS2563 , TAS2564

       

  • CONTENTS
  • SEARCH
  • Thermal Foldback Feature on SmartAmps
  1.   Advantages of Thermal Foldback on SmartAmps
    1.     Trademarks
    2. 1 Advantages of Thermal Foldback Feature
    3. 2 Temperature Monitor
    4. 3 Thermal Foldback Configuration
      1. 3.1 Temperature Threshold
      2. 3.2 Thermal Max Attenuation
      3. 3.3 Thermal Slope
      4. 3.4 Hold Time
      5. 3.5 Release Rate
    5. 4 Thermal Foldback Performance
      1. 4.1 Device Configuration
      2. 4.2 Thermal Foldback Disabled
        1. 4.2.1 Initial Temperature
        2. 4.2.2 Final Temperature
      3. 4.3 Thermal Foldback Enabled
        1. 4.3.1 Final Temperature
    6. 5 Conclusions
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Thermal Foldback Feature on SmartAmps

Advantages of Thermal Foldback on SmartAmps

The new generation of Texas Instruments SmartAmps, TAS2110, TAS2562, TAS2563 and TAS2564, introduce a new feature called Thermal Foldback. This feature allows the device to keep playing audio even when the temperature of the device is rising. Most audio amplifiers nowadays have thermal protection, which stops the audio playback or even shuts-down the device completely, so that it is not damaged due to high temperatures exposure. Thermal Foldback will automatically attenuate the output signal, by reducing the gain, letting the device cool-down while audio is still present at the output.

This application report is purposed to provide a thorough explanation of the Thermal Foldback functionality, how it can improve the end audio applications as well as show a comparison between the feature disabled and enabled.

Trademarks

All other trademarks are the property of their respective owners.

1 Advantages of Thermal Foldback Feature

Some audio applications, like automotive or industrial, require devices to operate in harsh environments where temperature is higher than consumer electronic goods typically endure. Most of the modern devices have protection schemes; however this typically stops the device from functioning or disables it completely. Once the temperature is back in a safe region, the device needs to be reinitialized.

Thermal Foldback feature on TAS2110, TAS2562, TAS2563 and TAS2564 has the advantage of allowing the device to keep operating and playing audio in increasing temperature situations. The device monitors the die temperature and automatically limits the audio signal above a set threshold. This will ultimately allow the device to keep or reduce its temperature while it is still operating. This is specially useful in fire & security applications as well as automotive applications where ambient temperature can be considerably higher than other applications but the system has to be fully operational. In any case, the over-temperature protection will shut down the device if the die temperature continually increases in order to prevent damages. In addition, over-temperature protection is an auto-retry feature so the device does not have to be reinitialized when temperature is back to a safe region.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale