The serial communication in TI's Programmable Logic Device (TPLD) enables the use of the USER register space. Using the USER register space allows for small adjustments of select fields, like counter blocks control data field, or can be used similar to I/O without having to go through device pins. The TPLD is currently only capable of being a The USER registers can be found under Detailed Description -> Device functional modes -> Programming -> “Device name” Registers -> “device name”_USER_REGISTER. For this application brief, the TPLD1202 is the device being used and any references to addresses are based on that devices USER register table.
Table 1 is an example of a USER register space. The table does not have all the options available in all devices, but is a large set of what can be available.
Acronym | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
---|---|---|---|---|---|---|---|---|
DEVICE_ID0 | DEVICE_ID_MSB | |||||||
DEVICE_ID1 | DEVICE_ID_LSB | |||||||
DEVICE_ID2 | DEVICE_ID_RSVD | |||||||
DEVICE_ID3 | DEVICE_ID_REV | |||||||
DEVICE_ID4 | DEVICE_ID4 | |||||||
DEVICE_ID5 | DEVICE_ID5 | |||||||
DEVICE_ID6 | DEVICE_ID6 | |||||||
DEVICE_ID7 | DEVICE_ID7 | |||||||
CNT0_COUNT | CNT0_COUNT | |||||||
CNT1_COUNT | CNT1_COUNT | |||||||
CNT2_COUNT | CNT2_COUNT | |||||||
CNT3_COUNT | CNT3_COUNT | |||||||
CNT4_COUNT_LSB | CNT4_COUNT_LSB | |||||||
CNT4_COUNT_MSB | CNT4_COUNT_MSB | |||||||
CNT5_COUNT_LSB | CNT5_COUNT_LSB | |||||||
CNT5_COUNT_MSB | CNT5_COUNT_MSB | |||||||
CNT6_COUNT | CNT6_COUNT | |||||||
CNT7_COUNT | CNT7_COUNT | |||||||
CNT8_COUNT | CNT8_COUNT | |||||||
CNT9_COUNT | CNT9_COUNT | |||||||
CNT0_DATA | CNT0_DATA | |||||||
CNT1_DATA | CNT1_DATA | |||||||
CNT2_DATA | CNT2_DATA | |||||||
CNT3_DATA | CNT3_DATA | |||||||
CNT4_DATA_LSB | CNT4_DATA_LSB | |||||||
CNT4_DATA_MSB | CNT4_DATA_MSB | |||||||
CNT5_DATA_LSB | CNT5_DATA_LSB | |||||||
CNT5_DATA_MSB | CNT5_DATA_MSB | |||||||
CNT6_DATA | CNT6_DATA | |||||||
CNT7_DATA | CNT7_DATA | |||||||
CNT8_DATA | CNT8_DATA | |||||||
CNT9_DATA | CNT9_DATA | |||||||
WATCHDOG_TIMEOUT_DATA | WATCHDOG_TIMEOUT_DATA | |||||||
WATCHDOG_OUTPUT_DATA | WATCHDOG_OUTPUT_DATA | |||||||
WATCHDOG_STATUS | WATCHDOG_STATUS | |||||||
PGEN_DATA_LSB | PGEN_DATA_LSB | |||||||
PGEN_DATA_MSB | PGEN_DATA_MSB | |||||||
STATE_MACHINE | RESERVED | CURRENT_STATE | ||||||
STATE0_OUT | STATE0_OUT | |||||||
STATE1_OUT | STATE1_OUT | |||||||
STATE2_OUT | STATE2_OUT | |||||||
STATE3_OUT | STATE3_OUT | |||||||
STATE4_OUT | STATE4_OUT | |||||||
STATE5_OUT | STATE5_OUT | |||||||
STATE6_OUT | STATE6_OUT | |||||||
STATE7_OUT | STATE7_OUT | |||||||
VREF_ACMP0 | VREF_ACMP0 | |||||||
VREF_ACMP1 | VREF_ACMP1 | |||||||
VREF_ACMP2 | VREF_ACMP2 | |||||||
VREF_ACMP3 | VREF_ACMP3 | |||||||
VREF_McACMP0_0 | VREF_McACMP0_0 | |||||||
VREF_McACMP0_1 | VREF_McACMP0_1 | |||||||
VREF_McACMP1_0 | VREF_McACMP1_0 | |||||||
VREF_McACMP1_1 | VREF_McACMP1_1 | |||||||
VREF_McACMP2_0 | VREF_McACMP2_0 | |||||||
VREF_McACMP2_1 | VREF_McACMP2_1 | |||||||
VREF_McACMP3_0 | VREF_McACMP3_0 | |||||||
VREF_McACMP3_1 | VREF_McACMP3_1 | |||||||
VIRTUAL_INPUT | VIRTUAL_IN | |||||||
VIRTUAL_OUTPUT | VIRTUAL_OUT | |||||||
SER_COMM_CFG | RESERVED | ADDR_AUTOINC | ||||||
CRC_STATUS | CRC_ERR_CNT | RESERVED | CRC_ERR_FLAG | |||||
SER_COMM_WR_MASK | SER_COMM_WR_MASK |
The DEVICE_ID registers are used to create an identity for each design. The first 2 DEVICE_ID registers are set by the device depending on the device selected for example the TPLD1202 has 0x12 in DEVICE_ID0 and 0x02 in DEVICE_ID1 where as the TPLD2001 has 0x20 in DEVICE_ID0, and 0x01 in DEVICE_ID1. DEVICE_ID 4 - 7 are loaded at startup with the Program ID written in the system settings within InterConnect Studio.
Starting from address 0 to address 7 are identifiers of the device. This includes the device id which based on the TI product number, for example. The TPLD1202 has register at address 0x00 = 0x12, and address 0x01 = 0x02 where as the TPLD2001 has 0x20, and 0x01 respectively. After that in registers DEVICE_ID 4-7 are loaded at startup with the Program ID. What this means is reading from Addresses 0-7 can have an entirely unique value to each design created by the user. Reading those registers not only provide which device is being used, but also which design is currently being loaded.
The CNTx_COUNT registers are read only registers that reflect whatever the current count of a counter block is. This can be used to give a rough estimate of how long a counter has left before reaching zero. It’s important to note that this read is asynchronous from the actual counter, so depending on when the value is read the counter can iterate before the value is return via the communication protocol.
The CNTx_DATA registers are read/write registers that store the value of control data written in InterConnect Studio. These values can be udated on the fly allowing the user to adjust PWM outputs, Increase/decrease delays, and adjust blocks like the frequency detectors on the fly.
The WATCHDOG portion of the register space allows the user to read the status, adjust the timeout period and output pulse length of the watchdog timer. The WATCHDOG_STATUS records how many times the watchdog has been triggered since startup or since the last read. This register is reset upon being read. Increasing the value in WATCHDOG_TIMEOUT_DATA increases the amount of time a signal can be low before an output pulse is triggered. Increasing the value of WATCHDOG_OUTPUT_DATA increases the length of the output pulse when the watchdog is triggered.
The STATE_MACHINE portion of the register space allows the user to control the current state and adjust each states behavior. SM_CURRENT_STATE contains the current state in binary format in bits 2-0. This is R/W so not only can the current state be read, but the serial controller can be used to force the state machine into certain states. This section also contains the state outputs listed as SM_S#_OUT_CFG. This allows the controller to adjust the outputs of any given state from this section.
the VREF portion of the register space allows the user to adjust the value going into the IN- of both multi-channel analog comparators and independent analog comparators. The value written here is not the value of the VREF, but rather what value the VREF is referencing. In the TPLD2001 the VREF steps by 32mV so increasing the value from 0x00 to 0x01 is changing that reference from 32mV to 64mV.
The VIRTUAL_INPUT register is used to store the values going into the TPLD device. This register is used to act as an optional inputs into the device. This can be used in place of pins to expand the output count of the controller.
The VIRTUAL_OUTPUT register is used to store the values going out of the TPLD device at any given time. Similar to the earlier CNT_COUNT registers mentioned above a read from this register is asynchronous, so after making the request and before the data is returned one of these values can possibly change.
The CRC_STATUS register is used to check if the device has started up correctly. The CRC_ERR_CNT section stores how many times the CRC process iterated before successful startup. The TPLD device is designed to run the CRC_ERR_CNT value up to 8 before full power on. If this value is at 8 and the CRC check fails the CRC_ERR_FLAG is flipped to 1. This register can be used to check if the design in the TPLD was successfully loaded, and if these values are unacceptable power cycle the device. If the device fails start-up again begin error analysis of your design attached to the TPLD.
The SER_COM_WR_MASK register is used to apply a mask over any future reads or writes. This can be used to read just the bottom half, or top half, of a register. The values not within the mask are all be read as 0 by the TPLD or returned as 0 to the controller.
Each TPLD has a specific set of pins that are tied to the serial communication which are initialized as the peripheral is added to the design. An example of a I2C setup can be seen in Figure 1, and an example SPI setup in Figure 2.
InterConnect Studio (ICS) is a software tool used to design, simulate, and configure the TPLD family of devices.
Figure 3 shows the initial setup of the I2C peripheral in InterConnect Studio. I2C can be added to the design by clicking the plus button indicated by the red arrow. The peripheral address is a binary value that can be used to statically set the address of this TPLD design. Below the peripheral address is a setting to enable an external pin-based address. Many I2C peripherals come with predefined addresses, but the TPLD does not, instead using these two settings allows many TPLDs to sit on an I2C bus without interfering with each other. Enabling the pin-based address allows for the peripheral address to be overwritten by the logic value present at the pin when the communication starts. The last setting unique to I2C is the Global Reset Listening which enables the device to be reset when a reset command is sent from the controller.
SPI has fewer options as SPI is not an addressable protocol as shown in Figure 4. The shared option of Virtual Inputs is used to allow the device to view the VIRTUAL_INPUT register. In some TPLD family devices the virtual inputs take the place of some pins as input to the connection matrix, and checking the data sheet clarifies which inputs are unable to be used together. For example in the TPLD1202 VIR_IN0 is shared with IO1 as shown in Table 2, meaning that IO1 cannot be used as an input pin into the design if VIR_IN0 is selected.
Virtual input | VIR_IN0 | VIR_IN1 | VIR_IN2 | VIR_IN3 | VIR_IN4 | VIR_IN5 | VIR_IN6 | VIR_IN7 |
Digital Input Pin | IO1 | IO2 | IO3 | IO4 | IO5 | IO6 | IO7 | IO9 |
A simple implementation of I2C can be using the TPLD1202 as an I/O expander as shown in Figure 5. Three pins are being used as digital inputs and being fed into the input side of the block. These pins are going to feed values into the VIRTUAL_OUTPUT register to be read during operation. Four pins are being used as digital outputs of the device, and are connected to VIR_IN0, VIR_IN1, VIR_IN2, VIR_IN3. These pins reflect the value present in the VIRTUAL_INPUT register, for example, pin4 (IO6) reflects bit 0 so on and so forth.
There is a PWM being run at 50% duty cycle by default. The KEEP input is held high so the duty cycle never changes unless the value of CNT_DATA is overwritten.
The setup for operation is shown in Figure 6 with the logic analyzer connections excluded. The TPLD-PROGRAM is used to update the design without requiring a burn of the device. Internal pull-ups are used within the USB2ANY during messaging.
To write to pins 4 to 7 we write the values to the internal address of VIRTUAL_INPUT (address: 0xE0). The USB2ANY explorer setup can be viewed in Figure 7, and an example of the operation can be viewed in Figure 8. The address entered into the Slave Address box appears different from the design because in the TPLD1202 the I2C receiver only uses 4 bits while the USB2ANY uses a 7 bit address. The address value entered has to be shifted to the left 3 bits from the value entered into ICS for the TPLD to be recognized. The only changes between commands was changing the value in the write data section before selecting Write.
To read from pins 0 to 2 we first do an empty write to the register VIRTUAL_OUTPUT (address: 0xE1) then execute a read command to the device. The USB2ANY explorer setup can be viewed in Figure 9, and an example of the operation can be viewed in Figure 10
Lastly to adjust the PWM write a new value to the register CNT6_DATA (address: 0x26). The USB2ANY explorer setup can be viewed in Figure 11, and an example of the operation can be viewed in Figure 12
Hardware used in support of this document can be found in Table 3
Device | EVM |
---|---|
All TPLD | TPLD-PROGRAM |
TPLD1202 | TPLD1202-DYY-EVMTPLD1202-RWB-EVM |
N/A | USB2ANY |