• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Supporting Time and Skew Sensitive Interfaces with TI's TXV Level-Shifter Portfolio

    • SCEA139 October   2023 TXV0106 , TXV0106-Q1 , TXV0108 , TXV0108-Q1

       

  • CONTENTS
  • SEARCH
  • Supporting Time and Skew Sensitive Interfaces with TI's TXV Level-Shifter Portfolio
  1.   1
  2.   2
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Application Brief

Supporting Time and Skew Sensitive Interfaces with TI's TXV Level-Shifter Portfolio

Introduction

Physical layer devices (PHYs) play an important part of the Ethernet network protocol as they bridge data communication from the external world by serializing and de-serializing data over many different types of translation media. PHYs are connected to an Ethernet media access controller (MAC), which is typically integrated in an FPGA or SoC. Interface design challenges often arise as large digital devices like SoCs, ASICs, and FPGAs move to lower core voltages. Integrated and standalone MACs are often not able to support a higher I/O voltage when operating at low voltages. System designers often need to resolve I/O level mismatch between the MAC and PHY while still maintaining the signal integrity of the interface. Additionally, Ethernet interfaces like Reduced Gigabit Media Independent Interface (RGMII) have strict timing requirements, which are even harder to meet at lower voltages.

This application brief provides over the timing requirements of RGMII and show how TI's high speed TXV family can meet RGMII timing requirements while overcoming I/O voltage mismatch.

RGMII Timing Requirements

RGMII is an interface used between the MAC and PHY and allows speeds of 10 Mbps, 100 Mbps and 1000 Mbps. Figure 1 shows the connection between the MAC and PHY. The timing requirements are more strict when operating at 1000 Mbps since data is processed in Dual Data Rate (DDR) signaling while the lower speeds use Single Data Rate (SDR). 1000 Mbps timing will be used throughout this app brief since satisfying those requirements also satisfies 10 Mbps and 100 Mbps timing requirements.

GUID-20230918-SS0I-TPCR-7FS6-NCRHFGZKD1WQ-low.svgFigure 1 RGMII Interface Between MAC and PHY

Table 1, Figure 2 and Figure 3, show the timing requirements for both RGMII Version 1.3 and 2.0 standards. Version 1.3 states skew must be introduced between the clock and data lines, typically around 1.5 to 2.0 ns. In Version 2.0, skew can be generated by either the MAC or PHY and are given by TsetupT and TholdT. RGMII Version 2.0 timing is highlighted in red.

Table 1 RGMII Version 1.3 and 2.0 Timing Specifications
Symbol Parameter Min Typical Max Units
TskewT Data to Clock Output Skew (at Transmitter) -500 0 500 ps
TskewR Data to Clock Input Skew (at Receiver) 1 1.8 2.6 ns
TsetupT Data to Clock Output Setup 1.2 2.0 ns
TholdT Data to Clock Output Hold 1.2 2.0 ns
TsetupR Data to Clock Input Hold 1.0 2.0 ns
TholdR Data to Clock Input Hold 1.0 2.0 ns
Tcyc Clock Cycle Duration 7.2 8 8.8 ns
Dcyc Duty Cycle for Gigabit 45 50 55 %
TR/TF Rise/Fall Time (20-80%) 0.75 ns
GUID-20230918-SS0I-PC8V-FDSB-G6XJTLTP0BXF-low.svg Figure 2 RGMII Version 1.3 and 2.0 Transmitter Timing Diagram
GUID-20230918-SS0I-RGXT-ND9S-NLQDG8XDDRCW-low.svg Figure 3 RGMII Version 1.3 and 2.0 Receiver Timing Diagram

TXV Output Skew Measurements

The output channel-to-channel skew, Tsk(o), value found in the data sheet uses two types of skew measurements to capture the worst-case skew, output and inverting skew. An illustration for both can be found in Figure 4.

GUID-20231010-SS0I-ZTQH-0ZJK-NN6QFM7PZ19D-low.svg Figure 4 Output Skew (TRR/TFF) and Inverting Skew (TRF/TFR) Measurements

Output skew is the skew difference between any two outputs of the same device at identical transitions while driving identical specified loads. Output skew measurements are given by TRR and TFF. Inverting skew is the skew difference between two outputs of the same device with opposite input transitions while driving identical specified loads. Inverting skew measurements are given by TRF and TFR.

TXV Timing Benefit

Table 2 gives the timing difference between the TXV family and the RGMII standard. The comparison below shows the worst case timing of the TXV does not exceed the maximum timing parameters of the RGMII standard. This leaves timing margin to the MAC, PHY and PCB, and shows the TXV product family is suitable to interface with RGMII, even at 1000 Mbps.

Table 2 Comparison Between TXV0106/TXV0108 and RGMII Timing Specification
Symbol Parameter TXV Max (1)(1) RGMII Max Units
Tsk(o) Output Channel-to-Channel Skew ± 317 ± 500 ps
TR/TF Rise/Fall Time (20-80%) 0.48 0.75 ns
Dcyc Duty Cycle ± 4 ± 5 %

Conclusion

Processors such as FPGA, SoC, and ASICs are moving to lower voltage I/Os benefiting customers by reducing power consumption. This can result in I/O voltage mismatch, however, many level-shifters are not capable in meeting strict timing requirements like rise/fall time, channel-to-channel skew and duty cycle distortion for skew sensitive interfaces. This application brief demonstrated how the TXV level-shifter family can bridge the I/O voltage gap while also delivering optimized AC performance and meeting strict timing requirements for low-skew interfaces like RGMII.

1.

VCCA = 1.8 V, VCCB = 3.3 V, CLoad = 5 pF, 250 Mbps for each data channel at 125°C

1. Different voltage and loading conditions can also be found in the timing section on the TXV0106 and TXV0108 data sheet
Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale