• Menu
  • Product
  • Email
  • PDF
  • Order now
  • When to Replace a Relay With a Multiplexer

    • SCDA036A May   2022  – June 2024 TMUX7612 , TMUX8212 , TMUXS7614D

       

  • CONTENTS
  • SEARCH
  • When to Replace a Relay With a Multiplexer
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Size Requirement
    1. 1.1 Optimized Layout and Control
  5. 2 Reliability Over Time
  6. 3 Power Consumption
  7. 4 Switching Speed and Hot Switching
  8. 5 Signal Isolation
  9. 6 Capacitance
  10. 7 On-Resistance and Flatness
  11. 8 Leakage Current
  12. 9 Integrated Protection
  13. 10Latch-up Immunity
  14. 11Galvanic Isolation
  15. 12Conclusion
  16. 13References
  17. 14Revision History
  18. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Application Note

When to Replace a Relay With a Multiplexer

Abstract

As many systems such as automated test and measurement and factory automation become smaller and more cost constrained, one potential for savings can come from shrinking the signal chain. Almost every system contains some type of switching and historically, mechanical relays were used. This implementation can be good from a performance perspective, but comes with a significant tradeoff on size, cost, and reliability. In more modern designs, Photorelays are often used instead of mechanical relays. These typically take a small hit on signal performance to drastically reduce size and cost while increasing reliability. Many systems can be further optimized by using TI's integrated Flat On-Resistance Multiplexers instead of Photorelays. In this application note, we go over the differences in performance, cost, size, and reliability between these three solutions.

Though these three devices can serve similar purposes, their internal designs are very different. Mechanical relays typically consist of an inductive coil and a physical switch. When current excites the coil, it becomes magnetic and pulls two pieces of metal together. Photorelays have a similar operation except instead of a coil, an LED is used to drive the gate of a MOSFET on/off. A multiplexer integrates multiple drivers and MOSFETs onto the same chip and drives the gate with a constant voltage source. As a result, Multiplexers save PCB space compared to Photorelay and mechanical relays.

 Equivalent Circuits (from
                        left to right): Mechanical Relay, Photorelay, Multiplexer Figure 1-1 Equivalent Circuits (from left to right): Mechanical Relay, Photorelay, Multiplexer

Trademarks

All trademarks are the property of their respective owners.

1 Size Requirement

One of the largest benefits to an integrated multiplexer switching design is size. For example, in a 16-channel system, 16 SPST (1:1) mechanical relays would be needed, accounting for >450mm2 board area. This is before including any relay driver ICs. Compare this to a Photorelay design and the user can see that the size requirements reduce dramatically. But Photorelays can not be driven directly through GPIO and need an LED driver to control the state of each switch. This adds to the design size and increases the system complexity, as well as power requirements. TI’s Multiplexer design such as the TMUX821x and TMUX7612 do not require any additional ICs. Each individual switch can be controlled by standard digital pins with 1.8V Logic. As a result, TI’s switch design is even smaller than a comparable Photorelay design.

 16 Channel, 50V design
                            Size Comparison (drawn to scale) Figure 1-1 16 Channel, 50V design Size Comparison (drawn to scale)
 TMUXS7614D top,
                            TMUX7612/TMUX8212 middle, Photorelay Bottom Figure 1-2 TMUXS7614D top, TMUX7612/TMUX8212 middle, Photorelay Bottom

As design size becomes a larger concern, routing and layout become a major consideration. The table below compares the actual design size of these three options with routing. You can see while the package density of the TMUX7612 and Photorelay are similar, when routing and layout is considered the space savings is more significant. And the TMUXS7614D saves significantly more area on top of this by integrating the passive components and optimizing the pinout.

Table 1-1 PCB Area Comparison for 16 channel design

TMUXS7614D
TMUX7612
TMUX8212
Photorelay
Total Package Area 2.5mm2/ch 4.0mm2/ch 4.2mm2/ch
Total PCB Area 3.18mm2/ch 9.13mm2/ch 11.22mm2/ch
Area Savings 129mm2 (70% reduction) 33.5mm2 (20% reduction) -

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale