• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Space-Grade, 50-krad, Overcurrent Event-Detection Circuit

    • SBOA512 April   2021 INA901-SP

       

  • CONTENTS
  • SEARCH
  • Space-Grade, 50-krad, Overcurrent Event-Detection Circuit
  1.   1
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

CIRCUIT DESIGN

Space-Grade, 50-krad, Overcurrent Event-Detection Circuit

Design Goals

InputOvercurrent ConditionsOutputSupply

Response Time

Total Ionizing Dose

Single Event Immunity

Iload MinIload MaxIOC_THVout_OCVS

tdelay

TID

SEL

5A10A11A2.2V5V

< 5µs

50 krad (Si)

75 MeV×cm2/mg

Design Description

This is a unidirectional current-sensing solution, generally referred to as overcurrent protection (OCP) that can provide an overcurrent alert signal to power off a system exceeding a threshold current. In this particular setup, the normal operating load is from 5A to 10A, with the overcurrent threshold defined at 11A (IOC_TH). The current shunt monitor and comparator are powered from a single 5-V supply rail. OCP can be applied to both high-side and low-side topologies. The solution presented in this circuit is a high-side implementation, with RL placed as a representation of a purely resistive system load at 4Ω. This circuit is useful in a variety of power applications for telemetry, health monitoring and system diagnostics. In addition to this functionality, this circuit implements the INA901-SP, which is a Radiation-Hardness-Assured (RHA), 50-krad(Si) capable device at Low Dose Rate, that is also Single Event Latch-up (SEL) Immune to 75 MeV-cm2/mg at 125°C. The comparator function is fulfilled by a LM193QML-SP, but the LM139AQML-SP can be used here as well, if additional comparator device count is needed.

GUID-20210305-CA0I-J6CV-FPQP-G12DD9THH4TH-low.gif

Design Notes

  1. For accurate comparator applications without hysteresis, it is important to maintain a stable power supply with minimized noise and glitches. To achieve this, use decoupling capacitors C1 and C2 to ensure device supplies are stable. Place the decoupling capacitors as close as possible to the supply pins of their respective devices. This should also be implemented on the negative supply of the comparator, if used.
  2. If a larger dynamic current measurement range is required with a higher trip point, a voltage divider from the INA901-SP OUT pin to ground can be incorporated with the divider output going to the LM193QML-SP input. Ensure that the designed range of the INA901-SP remains within the input common-mode specification of the LM193QML-SP.
  3. If additional short circuit to ground protection is needed in the circuit, fuses in series with the input pins can provide this functionality, but resistors should not be used for this purpose. Addition of resistors to the input pins of the INA901-SP will fundamentally change the gain of the amplifier. However, the tolerance of the internal resistors will fluctuate up to 30% (these resistors are matched to one another, rather than an absolute value), and thus this change in gain will vary from device to device, and cannot be considered reliable design.

Design Steps

  1. Full Scale Range: Determine the load range of conditions needing to be monitored. Choice of RSHUNT should be made with respect to the maximum range of current allowable to the input sense voltage, including the overcurrent value. Additional considerations are offset voltage on the lower end of measurement, and maintaining a valid common mode voltage on the input pins of the LM193QML-SP. While designing with INA901-SP, for best performance, ensure that the IMIN condition with the chosen shunt produces a sense voltage > 20mV to comply with the Accuracy Variations as a Result of VSENSE and Common-Mode Voltage section of the INA901-SP Radiation Hardened, –15-V to 65-V Common Mode, Unidirectional Current-Shunt Monitor Data Sheet.
  2. Gain Options: For the INA901-SP, only a 20V/V option is available, so this condition is fixed for this design.
  3. Choosing a shunt resistor: Given the design conditions, choose an appropriate shunt using the following equation. Note that there is a 200-mV reduction on the supply voltage to ensure that the device meets swing-to-rail limitations of the device. Numerical values come from the previously-defined use case:
    Equation 1. GUID-20210305-CA0I-WFV3-ZBFJ-ZN2H4JZJJ7HX-low.gif

    A shunt resistor value of 10mΩ is chosen for the design. Be aware that while a larger shunt provides more utilization of the full scale range, thermal constraints on the shunt will increase proportionally with the resistance. Selection of a higher value will also increase the voltage of the overcurrent trip point, which may cause challenges in satisfying the common-mode requirement of the LM193QML-SP.

  4. Setting the overcurrent point: From the INA901-SP, with the value of RSHUNT now determined, it is found that the output of the INA901-SP at the overcurrent point is:
    Equation 1. GUID-20210305-CA0I-NKQC-TMZV-TFVMHHJWNWWV-low.gif

    The overcurrent condition is set by a voltage divider between R2 and R3 set for the previously-mentioned point. Choose a value for R3 and calculate the needed resistor R2. Here, R3 is chosen at 10kΩ:

    Equation 1. GUID-20210305-CA0I-FMWT-TQ3V-WG26GNCNQJBK-low.gif

    Note that the LM193QML-SP requires that at least one input be from 0V to 3V when operating at a supply of 5V to satisfy the input common-mode requirement. This node held at a constant 2.2V satisfies this requirement for all values of comparison.

    Often, calculated resistor values will not directly align with available resistor choices. Here, 12.73kΩ is not a standard value, so the closest standard value of 12kΩ is selected. The actual overcurrent point based on the resistor value can be found by combining the previous equations.

    Equation 1. GUID-20210305-CA0I-VT6D-M5CB-FBZWQ2SRVL61-low.gif
  5. Offset error check: Check that the minimum meaningful current measurement is significantly higher than the current shunt monitor input offset voltage. The recommended maximum error from offset, eVOS is 10%. The value of eVOS can be lowered for tighter error targets:
    Equation 1. GUID-20210305-CA0I-P3JG-9GDV-SGMHMTWCDKFH-low.gif

    This value means that at a measured current of 3.5A for the chosen shunt, offset voltage will contribute a 10% error to the measurement.

Design Simulations

Transient Simulation Results

High-Side OCP Simulation Results

The first simulation examines the ramp response of the circuit, as the current transitions above the overcurrent trigger point.

GUID-20210305-CA0I-T8CB-VJHQ-VRPKN3MW0RXH-low.gifINA901-SP Overcurrent Ramp Response
GUID-20210305-CA0I-6T95-86TF-VMMGPC2WX2CS-low.gifINA901-SP Overcurrent Ramp Response, Zoom In

Next, examining the delay response of the circuit, with a step response delivered at 4.0ms, it is shown that the circuit responds to the event approximately 2.5µs later, so the delay response is satisfied:

GUID-20210305-CA0I-J3ZC-MHSF-KZDH5C96WFZ6-low.gifINA901-SP Overcurrent Protection Step Response

Design References

See the TI Precision Labs, Current Sense Amplifiers video series.

Design Featured Current Sense Amplifier
INA901-SP
VS2.7V to 16V
VCM–15V to 65V
VOUTGND+3mV to VS-50mV, typical
VOS±500μV, typical
Iq350μA, typical
IB±8μA, typical

TID Characterization (ELDRS-Free)

50krad (Si)

SEL Immune to LET

75 MeV-cm2/mg

https://www.ti.com/product/INA901-SP

For less harsh radiation environments, TI also offers the INA240-SEP, which offers Single Event Latch-up (SEL) Immunity to 43 MeV-cm2/mg at 125°C. It is ELDRS Free to 30 krad(Si), and Total Ionizing Dose (TID) RLAT for Every Wafer Lot is up to 20 krad(Si):

Table 1-1 Design Alternate Current Sense Amplifier
INA240-SEP
VS2.7V to 5.5V
VCM–4V to 80V
VOUTGND+1mV to VS-50mV, typical
VOS±5μV, typical
Iq1.8mA, typical
IB±90μA, typical

TID Characterization (ELDRS-Free)

30 krad (Si)

SEL Immune to LET

43 MeV-cm2/mg

https://www.ti.com/product/INA240-SEP
Table 1-2 Design Alternate Comparator

TLV1704-SEP

LM139AQML-SP

VS2.2V to 36V

2V to 36V

VCM

Rail-to-Rail

0V to 34V

VOUT

Open-Collector, Rail-to-Rail

Open-Collector

VOS

500μV

2mV

Iq

55μA/channel

200μA/channel

tPD(HL)

460ns

2.50μs

TID Characterization (ELDRS-Free)

30 krad (Si)

100 krad (Si)

SEL Immune to LET

43 MeV-cm2/mg

SEL Immune (Bipolar process)

https://www.ti.com/product/TLV1704-SEP

https://www.ti.com/product/LM139AQML-SP

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2020, Texas Instruments Incorporated

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale