This document describes the known exceptions to the functional and performance specifications to TI CMOS Radar Devices (AWR2944P, AWR2E44P, AWR2944-ECO, AWR2E44-ECO, AWR2944LC, AWR2E44LC ).
To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of Radar / millimeter Wave sensor devices. Each of the Radar devices has one of the two prefixes: XAs or AWR2xxx (for example XA2944PBGALT) ALT). These prefixes represent evolutionary stages of product development from engineering prototypes (XAs) through fully qualified production devices (AWR2xxx).
Device development evolutionary flow:
XAx — | Experimental device that is not necessarily representative of the final device's electrical specifications and may not use production assembly flow. |
AWR2xxx — | Production version of the silicon die that is fully qualified. |
XAs devices are shipped with the following disclaimer:
"Developmental product is intended for internal evaluation purposes."
Texas Instruments recommends that these devices not to be used in any production system as their expected end –use failure rate is still undefined.
Figure 3-1 shows an example of the AWR2944P/AWR2E44P Radar Device's package symbolization. AWR2944-ECO, AWR2E44-ECO, AWR2944LC, AWR2E44LC will have similar markings with 'E' and 'L' respectively in place of 'P' on line 1.
This identifying number contains the following information: