• Menu
  • Product
  • Email
  • PDF
  • Order now
  • IWR1443 Device Silicon ErrataSilicon Revisions 1.0, 2.0, and 3.0

    • SWRZ074C May   2017  – May 2021 IWR1443

       

  • CONTENTS
  • SEARCH
  • IWR1443 Device Silicon ErrataSilicon Revisions 1.0, 2.0, and 3.0
  1. 1Introduction
  2. 2Device Nomenclature
  3. 3Device Markings
  4. 4Usage Notes
    1. 4.1 MSS: SPI Speed in 3-Wire Mode Usage Note
    2. 4.2 Identification
  5. 5Advisory to Silicon Variant / Revision Map
  6. 6Known Design Exceptions to Functional Specifications
    1.     MSS#01
    2.     MSS#03A
    3.     MSS#04A
    4.     MSS#05A
    5.     MSS#06
    6.     MSS#07A
    7.     MSS#08
    8.     MSS#09
    9.     MSS#13
    10.     MSS#14
    11.     MSS#15
    12.     MSS#19
    13.     MSS#20
    14.     MSS#21A
    15.     MSS#22
    16.     MSS#23
    17.     MSS#24
    18.     MSS#25
    19.     MSS#26
    20.     MSS#27
    21.     MSS#28
    22.     MSS#29
    23.     MSS#30
    24.     MSS#31
    25.     MSS#32
    26.     MSS#33
    27.     MSS#35
    28.     MSS#37B
    29.     MSS#38A
    30.     MSS#39
    31.     MSS#40
    32.     MSS#43A
    33.     MSS#44
    34.     MSS#45
    35.     ANA#01
    36.     ANA#02
    37.     ANA#03
    38.     ANA#04
    39.     ANA#06
    40.     ANA#07
    41.     ANA#08A
    42.     ANA#10A
    43.     ANA#11A
    44.     ANA#12A
    45.     ANA#13B
    46.     ANA#15
    47.     ANA#16
    48.     ANA#17A
    49.     ANA#18B
    50.     ANA#20
    51.     ANA#21A
    52.     ANA#22A
    53.     ANA#24A
    54.     ANA#27
  7. 7Trademarks
  8. 8Revision History
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

ERRATA

IWR1443 Device Silicon ErrataSilicon Revisions 1.0, 2.0, and 3.0

1 Introduction

This document describes the known exceptions to the functional and performance specifications to TI CMOS Radar Devices (IWR1443).

2 Device Nomenclature

To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of Radar / mmWave sensor devices. Each of the Radar devices has one of the two prefixes: XIx or IWRx (for example: IWR1443FQAGABL). These prefixes represent evolutionary stages of product development from engineering prototypes (XI) through fully qualified production devices (IWR).

Device development evolutionary flow:

XI —Experimental device that is not necessarily representative of the final device's electrical specifications and may not use production assembly flow.
IWR —Production version of the silicon die that is fully qualified.

XI devices are shipped with the following disclaimer:

"Developmental product is intended for internal evaluation purposes."

Texas Instruments recommends that these devices not to be used in any production system as their expected end –use failure rate is still undefined.

3 Device Markings

Figure 3-1 shows an example of the IWR1443 Radar Device's package symbolization.

GUID-20A36790-6E14-4CA9-8791-98ECA9562BAD-low.gif Figure 3-1 Example of Device Part Markings

This identifying number contains the following information:

  • Line 1: Device Number
  • Line 2:Temperature and Security Grade
  • Line 3: Lot Trace Code
    • YM = Year/Month Code
    • PLLL = Assembly Lot
    • S = Assembly Site Code
  • Line 4:
    • 964 = IWR1443 Identifier
    • D = ES2.0
    • FC = ES3.0
    • BLANK = ES1.0
    • ABL = Package Identifier
    • G1 = "Green" Package Build (must be underlined)

4 Usage Notes

Usage notes highlight and describe particular situations where the device's behavior may not match presumed or documented behavior. This may include behaviors that affect device performance or functional correctness. These usage notes will be incorporated into future documentation updates for the device (such as the device-specific data sheet), and the behaviors they describe will not be altered in future silicon revisions.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale