This document provides information about utilizing the QuickTrack Control App to certify CC33xx devices according to Wi-Fi® standards. The document provides a high-level overview of the certification process.
Wi-Fi® is a registered trademark of Wi-Fi Alliance.
Linux® is a registered trademark of Linus Torvalds in the U.S. and other countries.
Windows® is a registered trademark of Microsoft Corporation in the United States and other countries.
All trademarks are the property of their respective owners.
The QuickTrack Control App is a Wi-Fi automation test tool utilized for Wi-Fi Certification. This user guide is intended to provide an overview of using the QuickTrack Control App with the CC33xx devices to certify end products. The required software and set-up steps vary slightly between Linux® and Windows® operating software.
Note that Git Bash for Windows must be downloaded when using a Windows operating system.
The source files required to build and use the QuickTrack Control App can be cloned or downloaded and extracted from GitHub. It is imperative that the tags and checkouts are verified to ensure that the correct version is downloaded.
After using one of the above options to acquire the source file, the installer specific to the operating system being used must be downloaded. Both installers can be found on ti.com at the link below. Make sure to involve the appropriate installer file that corresponds to the operating system being used (Windows or Linux).