• Menu
  • Product
  • Email
  • PDF
  • Order now
  • 433 to 930-MHz and 2.4-GHz BOM Tunable PCB Antenna

    • SWRA730 February   2022 CC1311P3 , CC1311R3 , CC1312R , CC1312R7 , CC1314R10 , CC1352P , CC1352P7 , CC1352R , CC1354P10 , CC1354R10

       

  • CONTENTS
  • SEARCH
  • 433 to 930-MHz and 2.4-GHz BOM Tunable PCB Antenna
  1.   Trademarks
  2.   Acronyms
  3. 1Description of the PCB Antenna
    1. 1.1 Implementation of the PCB Meander Monopole Antenna
    2. 1.2 Matching Network
  4. 2Test Setup
    1. 2.1 Radiation Pattern
  5. 3Unmatched Results
    1. 3.1 Smith Chart – Natural Impedance without Antenna Match Components
    2. 3.2 Smith Chart – Impedance with external component Z64
      1. 3.2.1 433 MHz Unmatched
      2. 3.2.2 470 MHz Unmatched
      3. 3.2.3 490 MHz Unmatched
      4. 3.2.4 510 MHz Unmatched
      5. 3.2.5 868/915 MHz Unmatched
  6. 4Single-Band Matching and Result
    1. 4.1 433-MHz Smith chart, SWR, Bandwidth, and Efficiency
    2. 4.2 470-MHz Smith chart, SWR, Bandwidth, and Efficiency
    3. 4.3 490-MHz Smith Chart, SWR, Bandwidth, and Efficiency
    4. 4.4 510-MHz Smith Chart, SWR, Bandwidth, and Efficiency
    5. 4.5 868/915-MHz Smith Chart, SWR, Bandwidth, and Efficiency
  7. 5Dual Band Matching and Results
    1. 5.1 433-MHz and 2440-MHz Smith Chart, SWR, Bandwidth, and Efficiency
    2. 5.2 470-MHz and 2440-MHz Smith Chart, SWR, Bandwidth and Efficiency
    3. 5.3 490 MHz and 2440 MHz Smith Chart, SWR, Bandwidth and Efficiency
    4. 5.4 510-MHz and 2440-MHz Smith Chart, SWR, Bandwidth, and Efficiency
    5. 5.5 868/915 and 2440-MHz Smith Chart, SWR, Bandwidth, and Efficiency
  8. 6Summary - Bill of Materials and Results
  9. 7Conclusion
  10. 8References
  11. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

433 to 930-MHz and 2.4-GHz BOM Tunable PCB Antenna

Trademarks

All trademarks are the property of their respective owners.

Acronyms

AcronymDefinition
AUTAntenna Under Test
BOMBill Of Materials
BWBandwidth
CFCorrection Factor
CITACellular Telecommunications Industry Association
DKDevelopment Kit

DNM

Do Not Mount

EBEvaluation Board
EIRPEffective Isotropic Radiated Power
EMEvaluation Module
ISMIndustrial, Scientific, Medical
NCNot Connected
NHPRPNear Horizon Partial Radiated Power
NHPRP45Near Horizon Partial Radiated Power within 45 degrees angle
OTAOver The Air
PCBPrinted Circuit Board
RFRadio Frequency
SWRStanding Wave Ratio
TRPTotal Radiated Power
VNAVector Network Analyzer

1 Description of the PCB Antenna

The antenna described in this document is a PCB meander monopole that users can configure by changing the BOM to operate as a single-band antenna or dual-band antenna. The resonance is set by the antenna PCB trace element and the antenna matching components. This allows the antenna to cover a wideband range with one antenna pattern design. The impedance of this antenna depends on the mode used. Referring to Figure 1-1, if the length of L4 is kept as shown, this is beneficial for operation around 433–510 MHz. If L4 is shortened to half the length (19.0 mm), this is beneficial when operating at 868–930 MHz.

The antenna layout is positioned on the top and bottom layer of the board as can be seen in Figure 1-1; this enables a lower resistive loss and gives a slightly wider bandwidth compared to a single-sided layout solution. With a single-sided layout; the area underneath the antenna can not be used for any other routing so it is more useful to utilize this area to optimize the antenna’s performance.

1.1 Implementation of the PCB Meander Monopole Antenna

To obtain optimum performance, it is important to make an exact copy of the antenna dimensions. The antenna was implemented on a 1.6-mm thick FR4 substrate. Since there is no ground plane beneath the antenna, the PCB thickness is not critical. If a different thickness is used then it could be necessary to change the matching network to obtain optimum performance.

One approach to implement the antenna in a PCB CAD tool is to import the antenna layout from a Gerber file. Refer to files included in the LAUNCHXL-CC1352P-4 Reference Design.

If the antenna is implemented on a PCB that is wider than the antenna it is important to avoid placing components or having a ground plane close to each side of the antenna. If the CAD tool being used does not support import of Gerber files, Figure 1-1 and Table 1-1 can be used.

GUID-20220119-SS0I-VSNC-4CBZ-DH6GKGGVTNCW-low.pngFigure 1-1 LAUNCHXL-CC1352P-4
Table 1-1 Antenna Dimensions
L116.0 mmL5

7.0 mm

L22.0 mmL6

1.4 mm

L324.0 mmL73.0 mm
L438.0 mmW2.0 mm

The last antenna segment's optimum length will always be dependent on the geometry of the ground plane. For ground plane sizes smaller than the LAUNCHXL-CC1352P-4 (less than a quarterwave), the optimum length of the last segment could be increased or the antenna match re-calculated for the new ground plane size.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale