This application report describes TI’s cascaded mmWave radar system. This solution is based on TI’s AWR2243 radar chip. Using the 20 GHz LO input and output paths, several of these chips are cascaded together and operated synchronously. Each AWR2243 chip supports up to four receive and three transmit antennas. Cascading multiple such chips allows the radar system to operate with more receive and transmit antennas, thereby improving target detection and resolution in comparison with a single AWR2243 radar chip based system. Cascading of two and four AWR2243 chips is illustrated in this application report. This cascaded radar solution is intended to support automotive applications such as Adaptive Cruise Control, Collision Warning, Emergency Braking, and Semi and Fully Autonomous Driving. The system described in this document has been implemented for evaluation in the mmWave cascade imaging radar RF evaluation module (https://www.ti.com/tool/MMWCAS-RF-EVM).
All other trademarks are the property of their respective owners.
Multiple AWR2243 chips may be cascaded on PCB to improve target detection and resolution. In this section, two chip cascading and four chip cascading systems are illustrated as examples. The focus is on connection of various signals that the AWR2243 chips need to share among themselves. Of the multiple AWR2243 chips in the cascaded system, one is referred to as the Master and the others as Slaves. To make the entire cascaded system operate as a single radar system, the Master is designated to generate a common Local Oscillator (LO) signal (19 GHz to 20.25 GHz) shared across all the transmitters and receivers in the entire cascade system. The master also controls the radar chirp/frame timing for all the chips by generating a digital Sync signal and sharing this synchronization signal with the slaves. The master also uses a 40 MHz crystal and generates a 40 MHz oscillator clock (OSC_CLKOUT) and shares it with the slaves (as CLKP), thereby eliminating the need for additional crystals on the slaves and ensuring that the entire system operates from a single clock source.
The master is capable of supplying the shared LO on two different output pins through two different delay matched amplifiers. This can be used in a four chip cascade system to supply the LO signal to the master and three slaves using only passive splitters. This eliminates the need for additional, costly, active components on the PCB. The OSC_CLKOUT pin is used by the master to share the the 40 MHz clock source with the slave devices in the system. In the case of a 2-device system, this can be done with just a passive trace between devices. In the case of more than 2-devices, it is recommended to use a clock fan-out buffer to manage loading and signal integrity issues. Similarly, the DIG_SYNC is conveyed from the master to the slaves and back to itself through delay matched buffers on board.
Other than these connections which are illustrated in the below diagrams and further elaborated in later sections, the cascaded system also has Power Management ICs (PMIC) (each PMIC can handle up to two AWR2243 chips), an optional QSPI Flash (needed for initial software development purpose only) and the mmWave antennas connected to each AWR2243 chip.
In a cascaded system, there is one Master chip and one or many Slave chips. These cascaded devices are synchronized using the following interfaces:
The 20 GHz (FMCW) RF LO is generated by the master chip and distributed to the slaves and the master. The relevant signals/pins are referred to as FM_CW_SYNCx/CLKx or 20 GHz LO in this document.
The frame timing synchronization is controlled by either the master chip, in the case of software message based frame trigger, or by the host processor, in the case of hardware based frame trigger. The relevant signals/pins are referred to as SYNC_IN/OUT or DIG_SYNC_IN/OUT in this document.
The 40 MHz system clock may be generated by either the master chip or externally supplied. The relevant pins are OSC_CLKOUT, CLKP and CLKM.
Detailed description on syncing is given in the following sections.