• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Duty Cycle Calculation in WEBENCH® Power Designer

    • SSZTCO3 may   2015 TPS54325-Q1

       

  • CONTENTS
  • SEARCH
  • Duty Cycle Calculation in WEBENCH® Power Designer
  1.   1
  2.   2
    1.     3
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Duty Cycle Calculation in WEBENCH® Power Designer

Pavani Jella

The duty cycle of a switching regulator is often thought of as being simply proportional to the input and output voltages. But when we look into the details of the calculations, we see that it also reflects circuit losses. Selecting components that give more losses, such as an inductor with a higher DCR, can cause the duty cycle to increase (for a buck converter), potentially resulting in additional efficiency loss from other components. When creating a power supply design with TI’s WEBENCH® Power Designer, the model calculations do not rely on basic ideal equations, but instead use detailed calculations that show you the interaction between component losses via small changes in duty cycle. To explore this, let’s look at an example of a buck converter as shown in Figure 1.

GUID-50363744-0E19-41F2-8DCE-532212B03687-low.png Figure 1 Asynchronous Buck Converter.

In a buck converter duty cycle D is defined as, D = Ton/Ts

Where Ts = 1/switching frequency

Ton = switch on-time

When the high-side power switch is turned on, current drawn from the input flows through the inductor. When the high-side switch is turned off, the diode (or low-side NMOS switch in this case of a synchronous converter) is turned on and current circulates through the diode (or low-side NMOS switch) since the inductor current cannot instantaneously stop. During the steady-state operation, the on and off times of the switch are balanced to maintain the desired output voltage. Figure 2 illustrates that during on-time of the switch, inductor current and the current through the high-side MOSFET ramps up, whereas, during the off-time of the switch, the diode and inductor currents ramp down.

GUID-43FC06E9-9ED8-4E22-81BF-06C3D85A8610-low.png Figure 2 Buck Converter Waveforms.

Through substitution, we can get an equation for duty cycle that appears dependent on input voltage, output voltage, and the FET and diode voltage drops. If the FET and diode voltage drops are small compared to the input and output voltage, the duty cycle equation further reduces to the ratio of Vout to Vin. 

GUID-FE7F90AD-80EC-4A0A-8DCB-2F9F797B102E-low.png
For an ideal synchronous buck converter, where there are no voltage drops across the switches or other losses, duty cycle is exactly the ratio of output voltage to input voltage.

GUID-317470B4-4466-41B0-848D-315433CF52F9-low.png
However, realistic calculation of duty cycle in a synchronous buck converter involves voltages across the high-side and low-side components. Thus, we have to return to the non-ideal case and include all the original terms:

GUID-1DB091C9-3831-4D9F-B730-9BB3684E4CCD-low.png

The voltage terms in the above equation are proportional to the output load current, Iout.

GUID-2B35B62D-2963-477D-BCE4-49748B425B1F-low.png
From the above equation observe that:

GUID-BD58C88B-73A5-48C6-A579-2B8182269EB7-low.png

WEBENCH Power Designer calculations are based on these realistic loss terms. To study the effect of Vin, Iout and DCR on the inductor during duty cycle, a design using TI’s TPS54325-Q1 4.5V to 18V input, 3A synchronous step-down converter was created with Vin=11.5-12.5 V  and Vout=3.3 V Vout @ 3A output current (see Figure 3).

GUID-939AF49E-234E-4873-821C-EFBFDE397B01-low.png Figure 3 TPS54325-Q1 Synchronous Step-down Converter Vin=11.5-12.5V and Vout of 3.3V @ 3A Iout Load
GUID-EDBFFB76-93F4-4354-9456-872D131088F3-low.png Figure 4 Notice That the Inductor Selected Is a TDK SPM6530T-2R2M with 2.2 uH Inductance and 19 mOhm DCR
GUID-26C58047-C27D-4EC1-B73A-02CC808BE486-low.png Figure 5 Calculated Operating Values of This Design, Including Duty Cycle of 28.8%, Efficiency of 86.3% and Inductor Power Dissipation L Pd of 0.22 W
GUID-3886D55A-44C5-4D7B-A531-7B0D98FD6CFE-low.png Figure 6 WEBENCH® Power Designer Charts That Confirm That:
GUID-7320DD39-878E-4D3A-A95A-50DA167810F1-low.png

To study the impact of DCR on duty cycle and efficiency let’s choose a Coilcraft inductor XAL4020-222MB with the same inductance of 2.2 uH and an increased DCR of 35 mOhm(Figure 7). View the design here.

GUID-7AF40010-9035-4F85-8CF4-DF4ACD2677CB-low.png Figure 7 Selection of Coilcraft Inductor XAL4020-222MB with the Same Inductance of 2.2 uH and an Increased DCR of 35 mOhm

With increase in DCR the duty cycle is now 29.2% and efficiency dropped to 84.9% as seen in Figure 8.

GUID-0EE523E5-AAE5-44BB-976D-D832194178B0-low.png Figure 8 OpVals with Inductor with 35mOhm DCR.

To see a more significant change, a CUSTOM inductor with higher DCR of 0.5 W and with same inductance is selected ( Figure 9). See the design here.

GUID-C502ECCA-C50A-44AB-AF5B-D3C076376414-low.png Figure 9 Setting of CUSTOM Inductor with 0.5Ohm DCR and Same Inductance 22uH

Note that now there is a significant jump in duty cycle to 40.4% and efficiency has dropped drastically to 57%. The drop in efficiency is due to a significant rise in inductor loss to 6.08 W. Figure 10 shows the steep increase in duty cycle and sharp drop in efficiency reiterating the same.

GUID-891F60FD-4BAE-4684-B788-DFA96DF2E8EC-low.png Figure 10 Efficiency and Duty Cycle Charts Showing the Effect of CUSTOM Inductor with High DCR of 0.5Ohm

Figure 11 and Figure 12 summarize the three DCR cases of 19 mW, 35 mW and 0.5 W of a 2.2 uH inductor, and its impact on duty cycle, efficiency and inductor power dissipation.

GUID-2DBB5648-27E9-4119-9F9E-365E20AC4394-low.png Figure 11 Comparison of OpVals for Three Cases of DCR
GUID-12FEC0DC-95BB-4A6C-B38E-6425E21CA8CA-low.png Figure 12 Summary of Charts for Efficiency, DutyCycle and L Pd

In conclusion, the switching regulator has to work extra hard to maintain the output voltage at the desired level with increase in DCR, which results in higher power dissipation losses. It’s thus important to choose an appropriate inductor with minimal DCR to maximize the efficiency of a switching regulator with an optimal duty cycle.

Start a design in WEBENCH today or watch a video tutorial on this topic.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale